Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Vivado Help on Zed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 556 views
  • Users 0 members are here
Related

Vivado Help on Zed

e14 Contributor
e14 Contributor over 10 years ago

Greetings everyone,

I'm working on a project with a ZedBoard, and I'm having a little trouble.  I'm primarily an embedded ARM developer, and I'm pretty to new Xilinx tools - and completely new to Vivado.  This is my first time using Zynq.

I've created a Block design that includes two AXI_Uart16550 cores and a clock wizard (the final design will include more uarts, but I'd like to get it working with two).  I need a very strange baud rate, which is the reason for the clock wiz.  During synthesis and implementation, I'm seeing some clocking failures and although I can produce a bitstream, things aren't working as I would expect.

Can anyone have a look at my vivado project and see if I've done something incorrectly?  I think I might have the processor resets wrong, but I'm not at all sure.

Any help would be greatly appreciated!

Vivado 2015.4 Project
https://file.io/d6cweS

James

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello James,

     

    Your link is broken.

     

    I would suggest adding your Zynq PS block and then your AXI Uart blocks to your block design and then using the 'Connection Automation' to generate the correct interconnection and resets.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Gary,

    That's strange.  It was working when I posted this.  Here's a new link: https://file.io/iNcEfp

    I appreciate you taking the time to respond.  That's pretty much what I did, but connection automation seemed to have a little trouble because of the clocking wizard in the mix.

    I just can't figure out why its failing some clocking - the design isn't super high speed (Clocking wizard of 49.152Mhz) and isn't very complex (low resource utilization).

    If you can get the file and provide any insight, I'd sure apprecaite it.

    James

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Looks like file.io is having some .. issues..
    Here's a link that should actually work: http://www.filedropper.com/zedcollectorxpr

    And one more from file.io to try since they're much faster: https://file.io/aW7vZc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello James,

     

    I took a quick look at your block design. It looks like you are clocking the AXI interface with the output of your clock wizard. Not sure why you would want to do that. If all you want is a custom baud rate the simplest thing to do would be to configure the axi_uart16650 IP to use an external clock and let the axi interfaces clock as usual with the fclk_clk0 outputs.

     

    You may not even need a clock wizard. Depending on your frequency requirements (input clock does need to be 1/2 axi clock or less)  you might be able to just enable one of the other PL fabric clocks (FCLK_CLKK1) to the input required for the baud rate generator and use that output. To do this you would re-customized the Zynq PS block, select Clock Configuration and enable and set a second PL Fabric Clock.

     

    -Gary