Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Add sources and libraries to a custom peripheral
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 360 subscribers
  • Views 1020 views
  • Users 0 members are here
Related

Add sources and libraries to a custom peripheral

Former Member
Former Member over 13 years ago

Hello,

I want to create a custom peripheral to use OLED on Zedboard. I reused this project: http://www.zedboard.org/node/511
This project uses the core "charLib" (files are already included in the project).

I do the following steps:
- in XPS, create a new IP, named "zedoled"
- change zedoled.vhd and user_logic.vhd with new connections to the other modules
- re-import my IP, including libraries (proc_common_..., axi_lite_ipif_...) and all VHDL files
- add my IP to my design
- Ports: connect to external port
- go back to PlanAhead, create Top Hdl and create ucf file
- generate bitstream

The problem: Synthesis is OK, but during Implementation, the module charLib cannot be resolved, even so this module is described in charLib.vhd that I included when re-importing my IP.
It 's strange because all other modules are recognized successfully... I'm sure that names match correctly and I'm sure the file is including in the sources.

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    Hi

    Have you added the additional files to the .pao file in the data folder?

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    Yes, I have the following line in the .pao file:
    lib zedoled_v1_00_a charLib vhdl

    And PlanAhead says:
    [Designutils 20-1022] Could not resolve non-primitive black box cell 'charLib' instantiated in module 'proc_module_i/zedoled_0/zedoled_0/USER_LOGIC_I/OLED_CTRL_0/Example/CHAR_LIB_COMP'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    OK, how did you re-import the IP?  XPS can be a bit tricky so I use the mpd and pao files in the Import Peripheral Wizard.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    I import the IP using only the vhdl files. Maybe that's the problem. I will try an other way.
    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    I have finally found the solution:
    I included the charLib.vhdl file in my sources. This is wrong. charLib must be used as a blackbox, so the netlist file must be used instead: charLic.ngc.
    During peripheral importation, at "source file type" window, check "HDL source files" and "Netlist files" boxes. The netlist file is added after the HDL sources.

    But I still don't understand why the module charLib could not be resolved whereas it is described it the vhdl file...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 13 years ago

    Hi vcesson,

    Can you please post the contents of your .pao file for the community to look at?

    I seem to remember that the list order of the dependency files in the Peripheral Analysis Order file is important.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago

    PAO file:
    ##############################################################################
    ## Filename:          C:XilinxProjectszedoled_charlibzedoled_charlib.srcssources_1edkproc_modulepcores/PmodOLEDCtrl_v1_00_a/data/PmodOLEDCtrl_v2_1_0.pao
    ## Description:       Peripheral Analysis Order
    ## Date:              Tue Mar 19 14:27:38 2013 (by Create and Import Peripheral Wizard)
    ##############################################################################

    lib PmodOLEDCtrl_v1_00_a Delay vhdl
    lib PmodOLEDCtrl_v1_00_a OledExample vhdl
    lib PmodOLEDCtrl_v1_00_a OledInit vhdl
    lib PmodOLEDCtrl_v1_00_a PmodOLEDCtrl vhdl
    lib PmodOLEDCtrl_v1_00_a SpiCtrl vhdl



    BBD file:
    ##############################################################################
    ## Filename:          C:XilinxProjectszedoled_charlibzedoled_charlib.srcssources_1edkproc_modulepcores/PmodOLEDCtrl_v1_00_a/data/PmodOLEDCtrl_v2_1_0.bbd
    ## Description:       Black Box Definition
    ## Date:              Tue Mar 19 14:27:38 2013 (by Create and Import Peripheral Wizard)
    ##############################################################################

    Files
    ################################################################################
    charLib.ngc


    Also I have the following line in my MPD:
    OPTION RUN_NGCBUILD = TRUE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago

    Thank you for that vcesson, you saved me, I could not find any other info anywhere on how to import a peripheral that contains other cores. In my case I was trying to import a peripheral with a block RAM core and was going crazy with this error.

    While I was able to finally work around this using vcesson's solution (i.e. import the .ncd file for the other core, but NOT the .v/.vhd file!), however the compiler was still complained about not finding the HDL file. What I ended up doing was simply pasting in the entire IP Core functional model directly into my peripheral code so that I only end up with a single file. Works for now, in the future should really find a better solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer