Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Add sources and libraries to a custom peripheral
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 354 subscribers
  • Views 864 views
  • Users 0 members are here
Related

Add sources and libraries to a custom peripheral

Former Member
Former Member over 13 years ago

Hello,

I want to create a custom peripheral to use OLED on Zedboard. I reused this project: http://www.zedboard.org/node/511
This project uses the core "charLib" (files are already included in the project).

I do the following steps:
- in XPS, create a new IP, named "zedoled"
- change zedoled.vhd and user_logic.vhd with new connections to the other modules
- re-import my IP, including libraries (proc_common_..., axi_lite_ipif_...) and all VHDL files
- add my IP to my design
- Ports: connect to external port
- go back to PlanAhead, create Top Hdl and create ucf file
- generate bitstream

The problem: Synthesis is OK, but during Implementation, the module charLib cannot be resolved, even so this module is described in charLib.vhd that I included when re-importing my IP.
It 's strange because all other modules are recognized successfully... I'm sure that names match correctly and I'm sure the file is including in the sources.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    I have finally found the solution:
    I included the charLib.vhdl file in my sources. This is wrong. charLib must be used as a blackbox, so the netlist file must be used instead: charLic.ngc.
    During peripheral importation, at "source file type" window, check "HDL source files" and "Netlist files" boxes. The netlist file is added after the HDL sources.

    But I still don't understand why the module charLib could not be resolved whereas it is described it the vhdl file...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    I have finally found the solution:
    I included the charLib.vhdl file in my sources. This is wrong. charLib must be used as a blackbox, so the netlist file must be used instead: charLic.ngc.
    During peripheral importation, at "source file type" window, check "HDL source files" and "Netlist files" boxes. The netlist file is added after the HDL sources.

    But I still don't understand why the module charLib could not be resolved whereas it is described it the vhdl file...