Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design programming the FPGA on zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 743 views
  • Users 0 members are here
Related

programming the FPGA on zedboard

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I wanted to know how could I program the FPGA on the zedboard, as i have tried to program it with adapt it was not possible. I have a VGA display code which was originally implemented for sparten 6 board,trying to implement the same on zedboard. I want to program just the FPGA not the arm processor. any ideas, hints will be helpful.

thank you ......

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you are using ISE you can use IMPACT, it is launched by the "Configure Target Device" process.

    I'm at work, but IIRC here is the process:

    - Power on Zedboard.

    - attach cable to micro-USB port at back left

    - Start Impact

    - Initalise the JTAG chain (CTRL+I is the keystroke)

    - Rightclick on the main canvas and select boundary scan.

    - When presented with the options for the PS (ARM processor) select "Bypass"

    - When presented with the ooptions for the PL (FPGA section) choose your bit file.

    - Right-click on the PS section icon and choose "program".

    I only ever have used a Zedboard with Impact, so there might be an additonal step to select which cable is in use - if so I've only done it once and don't remember.

    If you still have a problem let me know and I'll actually do it for real...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Another option would be to 'export' your design (including bitstream) to the SDK, even if you don't plan to run an application on the Zynq processor, and use the 'Program FPGA' option under the 'Xilinx Tools' SDK tool bar selection.

     

    Ultimately you will need to build at least a minimal Zynq project to load the bitstream of you plan to have your design boot from non-volatile memory and run without using the JTAG interface.

     

    -Gary