Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Problem in Flashing Boot from QSPI in ZEDBOARD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1356 views
  • Users 0 members are here
Related

Problem in Flashing Boot from QSPI in ZEDBOARD

e14 Contributor
e14 Contributor over 10 years ago

Hello all,

I am quite new in hardware design. I am trying to boot a 8-bit shift-register topology written in VHDL from the QSPI memory of the Zedboard. Booting from SD card is successfully completed; but the problem is that I am not able to complete booting it from QSPI. Since the source is a VHDL code, it cannot be exported as a design and no .ELF files are being created. The guide that I used during the flashing process is "Zedboard_boot_guide_IDS141_1_v1_1.pdfu201D.

I'm sorry if there is a duplicate in the forum.

Thanks in advance for your help.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Necati,

     

    The document you refer to is very dated and targets the older Xilinx ISE tool suite. I would suggest that you begin using the current Xilinx Vivado tool suite. The Zynq device on the ZedBoard is supported by the free WebPack Vivado version.

     

    That said I am a little confused about what you are trying to do. Creating a bootable image for either the SD Card or QSPI device requires a minimal Zynq PS (Processor System) design along with your PL (Programmable Logic) design. You would then export this to the SDK and generate an FSBL (First Stage Boot Loader), either a .bin file for SD Card boot or a .mcs file for QSPI boot.

     

    There is a good set of four tutorials that take you though this process posted on the MicroZed Reference Designs page. Tutorial 4 in particular details generating a bootable image. While it targets the MicroZed board you only need to change the board targeted to use with the ZedBoard:

     

    http://zedboard.org/support/design/1519/10

     

    Adam Taylor also has a really good series of blog posts that detail designing with Zynq based boards:

     

    http://zedboard.org/content/microzed-chronicles

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Necati,

     

    The document you refer to is very dated and targets the older Xilinx ISE tool suite. I would suggest that you begin using the current Xilinx Vivado tool suite. The Zynq device on the ZedBoard is supported by the free WebPack Vivado version.

     

    That said I am a little confused about what you are trying to do. Creating a bootable image for either the SD Card or QSPI device requires a minimal Zynq PS (Processor System) design along with your PL (Programmable Logic) design. You would then export this to the SDK and generate an FSBL (First Stage Boot Loader), either a .bin file for SD Card boot or a .mcs file for QSPI boot.

     

    There is a good set of four tutorials that take you though this process posted on the MicroZed Reference Designs page. Tutorial 4 in particular details generating a bootable image. While it targets the MicroZed board you only need to change the board targeted to use with the ZedBoard:

     

    http://zedboard.org/support/design/1519/10

     

    Adam Taylor also has a really good series of blog posts that detail designing with Zynq based boards:

     

    http://zedboard.org/content/microzed-chronicles

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer