Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Problem in Flashing Boot from QSPI in ZEDBOARD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1348 views
  • Users 0 members are here
Related

Problem in Flashing Boot from QSPI in ZEDBOARD

e14 Contributor
e14 Contributor over 10 years ago

Hello all,

I am quite new in hardware design. I am trying to boot a 8-bit shift-register topology written in VHDL from the QSPI memory of the Zedboard. Booting from SD card is successfully completed; but the problem is that I am not able to complete booting it from QSPI. Since the source is a VHDL code, it cannot be exported as a design and no .ELF files are being created. The guide that I used during the flashing process is "Zedboard_boot_guide_IDS141_1_v1_1.pdfu201D.

I'm sorry if there is a duplicate in the forum.

Thanks in advance for your help.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Necati,

     

    You have it pretty much correct. You need to make sure that when you export the hardware design to SDK you check the "include bitstream'" option. You do not need to assign any connections between the PS and the PL if your VHDL is a hardware only block with no interface to the Zynq PS. You just need to include a minimal Zynq PS IP block as shown in the tutorials. The Zynq PS block is required to boot the device and load the bitstream. Then just generate your FSBL and include the FSBL .elf file, then the .bit file, and finally any application .elf file when you generate your .mcs file for programming the QSPI.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Necati,

     

    You have it pretty much correct. You need to make sure that when you export the hardware design to SDK you check the "include bitstream'" option. You do not need to assign any connections between the PS and the PL if your VHDL is a hardware only block with no interface to the Zynq PS. You just need to include a minimal Zynq PS IP block as shown in the tutorials. The Zynq PS block is required to boot the device and load the bitstream. Then just generate your FSBL and include the FSBL .elf file, then the .bit file, and finally any application .elf file when you generate your .mcs file for programming the QSPI.

     

    -Gary