Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Which is the easiest way to connect a PL to System
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 725 views
  • Users 0 members are here
Related

Which is the easiest way to connect a PL to System

e14 Contributor
e14 Contributor over 13 years ago

Hi all, i am new in the forum and noobie in Hardware Deasing. I have a simple Ipcore that is running and works perfect, it has a 32 bit interface. I wondering which the easiest way to connect this to my PL and system. For example, suppose i have a simple dual port ALU and i want to use it in linux, my work is to build the driver.Which is the fastest way (developing time) to do this?. As far as i can see, the easiest way to do this is to map the 2 inputs of the ALU to a some region in memory. Is possible?
Thanks and sorry for my bad English.
-Alfonso

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Xillybus will soon release a version for Zynq. This means a plain FIFO on the PL, and a plain device file on the Linux machine. Just like the existing PCIe version.

    The bundle will include a ready-to-run Linux package, so it's load and go. And no hassling with the kernel.

    For the general idea, please visit http://xillybus.com.

    And yes, there's a slight self-promotion in this post, but hey, it answers the question. ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Xillybus will soon release a version for Zynq. This means a plain FIFO on the PL, and a plain device file on the Linux machine. Just like the existing PCIe version.

    The bundle will include a ready-to-run Linux package, so it's load and go. And no hassling with the kernel.

    For the general idea, please visit http://xillybus.com.

    And yes, there's a slight self-promotion in this post, but hey, it answers the question. ;)