Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard power up fail
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 362 subscribers
  • Views 3680 views
  • Users 0 members are here
Related

Zedboard power up fail

blake_ding
blake_ding over 7 years ago

Hi sir,

When I power on the Zedboard, the LD13(power) doesn't light and LD0 ~ LD7 all RED.

The only action was that I shorted the 3.3V of J18.
After that, the Zedboard seems crashed?

Could I reset it by myself?

BR
Blake

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 7 years ago

    Hi Blake,

    Can you take a look at some of the outputs with a multimeter and let me know if they are powering up? Unfortunately there are no easy test points, we'll have to look across the output caps. Do you have any other boards plugged in to the PMOD or FMC headers?

     

    here is the schematic link - http://zedboard.org/sites/default/files/documentations/ZedBoard_RevD.2_Schematic_130516.pdf

    5V - C391

    1.0V - C356

    1.8V - C365

    3.3V - C334

    Vadj - C339

    1.5V - C351

    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blake_ding
    0 blake_ding over 7 years ago in reply to ctammann

    Hi Chris,

    The result of measurement as below :

    5V - C391 (5V ok)

    1.0V - C356 (1V ok)

    1.8V - C365 (I can't find this component, can you help to highlight it's location?)

    3.3V - C334 (3.3V ok)

    Vadj - C339 (it's 0)

    1.5V - C351 (1.5V ok)

    ------------------------------------

    I got a HDMI-FMC, when I plugged it on FMC slot and connect to the display output of NB; I can see the LD1 is turned on.

    BR
    Blake

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ctammann
    0 ctammann over 7 years ago in reply to blake_ding

    Hey Blake,

    IS the jumper to set the output for Vadj in place? Was it set to the right level when it was first powered up with the FMC card attached? The 1.8V supply is most likely active as it's Power Good signal is used to turn on the other supplies.

    You could also look across C340 or on the output side of L3. My initial thought would be that Vadj was set to the wrong voltage level with something attached to the FMC and possibly damaged that output. That may not be the case, but it the most likely culprit if the other supplies are starting up properly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 7 years ago in reply to blake_ding

    Hey Blake,

    IS the jumper to set the output for Vadj in place? Was it set to the right level when it was first powered up with the FMC card attached? The 1.8V supply is most likely active as it's Power Good signal is used to turn on the other supplies.

    You could also look across C340 or on the output side of L3. My initial thought would be that Vadj was set to the wrong voltage level with something attached to the FMC and possibly damaged that output. That may not be the case, but it the most likely culprit if the other supplies are starting up properly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • blake_ding
    0 blake_ding over 7 years ago in reply to ctammann

    Actually, my original purpose is to verify the input of HDMI-FMC; and I refer to following website to :
    https://forums.xilinx.com/t5/Xcell-Daily-Blog-Archived/Adam-Taylor-s-MicroZed-Chronicles-Part-211-Working-with-HDMI/ba-p/786166

    Therefore, yes, I plugged HDMI-FMC and soldered the 3v3 of J18; then power up the Zedboard.
    After that, the Zedboard can't boot normally.

    No matter I replaced the jumper to 2v5 or 1v8 of J18, the C340 and L3 are both 0V.

    Could we rework the zedboard ourselves to recover it?

    BR
    Blake