Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Eth1 Gmii to Rgmii
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1273 views
  • Users 0 members are here
Related

Eth1 Gmii to Rgmii

e14 Contributor
e14 Contributor over 10 years ago

I am currently trying to implement an ethernet driven algorithm in the Zedboard. The board will interface with a GigE Vision Camera and I want to pull Ethernet packets directly into the Programmable Logic.
I understand that you need an external PHY that you provide ( I have one ordered). I am not fully understanding how to utilize the "GMII to RGMII v3.0" IP Core that Xilinx provides. I am not sure where that is sending the information.

It gives a gmii interface to the EMIO, but where do I access that data? I'm using Vivado 2014.2 and using the block design I can't see where the data will be accessed from the PS. When you switch the Eth1 peripheral to EMIO, it creates a GMII port in the processing system. This connects to the GMII port of the IP core.

Do you connect whatever customized IP you create to that same connection? Any information on how to correctly use this IP would be great.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 10 years ago

    You may also want to review the Ethernet designs that Opsero offers. They have an FMC with four Gigabit Ethernet ports, using a variety of PS IP (GEM1) and PL IP.

    www.ethernetfmc.com 

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 10 years ago

    You may also want to review the Ethernet designs that Opsero offers. They have an FMC with four Gigabit Ethernet ports, using a variety of PS IP (GEM1) and PL IP.

    www.ethernetfmc.com 

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    Thanks Bryan. I actually have ordered the FMC from them and will be trying to use one of the example designs when it arrives.