Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design GPIO/CAN Pins on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 1473 views
  • Users 0 members are here
Related

GPIO/CAN Pins on ZedBoard

e14 Contributor
e14 Contributor over 11 years ago

Please forgive me if this question has already been answered elsewhere.  I have a ZedBoard on which I am developing, and I require integration with a CAN bus.  The ZedBoard does not appear to break out the CAN bus.

I have, however, seen several posts on this forum about operating the CAN bus on a ZedBoard.  Some people seem to have been operating CAN over GPIO pins.

Are there any exposed CAN pins?  Are there any exposed GPIO pins that can be used to implement CAN over GPIO?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Take a look at the ARM System Level Control Registers section ( Appendix B.28 in the Zynq TRM, UG585 is a good place to start) of the Technical Reference Manual for Zynq. These configurations are controlled by the ARM System Registers. As an example, MIO Pin 14 I/O is selected by the MIO Pin 14 Control Register at address 0x00000738. You can read the state set by the ps7_init.c (or ps7_init.tcl for JTAG boot) but you should be very careful to understand the complete configuration state before changing register values.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Take a look at the ARM System Level Control Registers section ( Appendix B.28 in the Zynq TRM, UG585 is a good place to start) of the Technical Reference Manual for Zynq. These configurations are controlled by the ARM System Registers. As an example, MIO Pin 14 I/O is selected by the MIO Pin 14 Control Register at address 0x00000738. You can read the state set by the ps7_init.c (or ps7_init.tcl for JTAG boot) but you should be very careful to understand the complete configuration state before changing register values.

     

    -Gary