Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Adding a VDMA to a design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1172 views
  • Users 0 members are here
Related

Adding a VDMA to a design

Former Member
Former Member over 11 years ago

I have a design running on the Zedboard. It is based on the FMC- IMAGEON Vita Pass through tutorial. I have taken this design and modified it. I want to further modify it by adding a VDMA so that I can cope with different resolutions and frame rates.I am following the design guide lines in the LogiCORE IP Video In to AXI4-Stream v3.0 and the AXI Video Direct Memory Access v6.1. I have added the VDMA to the design and I get the following errors:

ERROR: [BD 41-237] Bus Interface property FREQ_HZ does not match between /processing_system7_0_axi_periph/s01_couplers/auto_pc/S_AXI(100000000) and /axi_vdma_0/M_AXI_MM2S(142857132)

ERROR: [BD 41-237] Bus Interface property CLK_DOMAIN does not match between /processing_system7_0_axi_periph/s01_couplers/auto_pc/S_AXI(zed_hdmi_processing_system7_0_0_FCLK_CLK0) and /axi_vdma_0/M_AXI_MM2S(zed_hdmi_processing_system7_0_0_FCLK_CLK1)

CRITICAL WARNING: [BD 41-237] Bus Interface property TDATA_NUM_BYTES does not match between /fmc_imageon_hdmio_rgb/v_rgb2ycrcb_0/video_in(3) and /axi_vdma_0/M_AXIS_MM2S(4)


ERROR: [BD 41-237] Bus Interface property FREQ_HZ does not match between /axi_vdma_0/S_AXIS_S2MM(100000000) and /fmc_imageon_vita_color/v_cfa_0/video_out(142857132)

ERROR: [BD 41-237] Bus Interface property CLK_DOMAIN does not match between /axi_vdma_0/S_AXIS_S2MM(zed_hdmi_processing_system7_0_0_FCLK_CLK0) and /fmc_imageon_vita_color/v_cfa_0/video_out(zed_hdmi_processing_system7_0_0_FCLK_CLK1)

Are there any good examples that will show me how to connect up the VDMA?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    I have already done that. In this design the VDMA doesn't have a video input. I'm want to know how to configure the VDMA when using the video input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    I have already done that. In this design the VDMA doesn't have a video input. I'm want to know how to configure the VDMA when using the video input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data