Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Adding a VDMA to a design
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 358 subscribers
  • Views 1164 views
  • Users 0 members are here
Related

Adding a VDMA to a design

Former Member
Former Member over 11 years ago

I have a design running on the Zedboard. It is based on the FMC- IMAGEON Vita Pass through tutorial. I have taken this design and modified it. I want to further modify it by adding a VDMA so that I can cope with different resolutions and frame rates.I am following the design guide lines in the LogiCORE IP Video In to AXI4-Stream v3.0 and the AXI Video Direct Memory Access v6.1. I have added the VDMA to the design and I get the following errors:

ERROR: [BD 41-237] Bus Interface property FREQ_HZ does not match between /processing_system7_0_axi_periph/s01_couplers/auto_pc/S_AXI(100000000) and /axi_vdma_0/M_AXI_MM2S(142857132)

ERROR: [BD 41-237] Bus Interface property CLK_DOMAIN does not match between /processing_system7_0_axi_periph/s01_couplers/auto_pc/S_AXI(zed_hdmi_processing_system7_0_0_FCLK_CLK0) and /axi_vdma_0/M_AXI_MM2S(zed_hdmi_processing_system7_0_0_FCLK_CLK1)

CRITICAL WARNING: [BD 41-237] Bus Interface property TDATA_NUM_BYTES does not match between /fmc_imageon_hdmio_rgb/v_rgb2ycrcb_0/video_in(3) and /axi_vdma_0/M_AXIS_MM2S(4)


ERROR: [BD 41-237] Bus Interface property FREQ_HZ does not match between /axi_vdma_0/S_AXIS_S2MM(100000000) and /fmc_imageon_vita_color/v_cfa_0/video_out(142857132)

ERROR: [BD 41-237] Bus Interface property CLK_DOMAIN does not match between /axi_vdma_0/S_AXIS_S2MM(zed_hdmi_processing_system7_0_0_FCLK_CLK0) and /fmc_imageon_vita_color/v_cfa_0/video_out(zed_hdmi_processing_system7_0_0_FCLK_CLK1)

Are there any good examples that will show me how to connect up the VDMA?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Hi,

    The errors you are getting should be quite easy to fix, it seems that you have simply swapped the clock connections on the VDMA between the MM2S and S2MM connections and therefore the clock domains are wrong.

    The critical warning is telling you that the VDMA is sending 4 bytes of data but the rgb2ycrcb module is only reading 3, you can use an AXIS data width converter to sort this out.

    For examples I would suggest Xapp794, it applies to the ZC702 but you should be able to use the same hardware architecture.

    http://www.xilinx.com/support/documentation/application_notes/xapp794-1080p60-camera.pdf

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Hi,

    The errors you are getting should be quite easy to fix, it seems that you have simply swapped the clock connections on the VDMA between the MM2S and S2MM connections and therefore the clock domains are wrong.

    The critical warning is telling you that the VDMA is sending 4 bytes of data but the rgb2ycrcb module is only reading 3, you can use an AXIS data width converter to sort this out.

    For examples I would suggest Xapp794, it applies to the ZC702 but you should be able to use the same hardware architecture.

    http://www.xilinx.com/support/documentation/application_notes/xapp794-1080p60-camera.pdf

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data