Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Shared data cache between PS and custom IP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 456 views
  • Users 0 members are here
Related

Shared data cache between PS and custom IP

e14 Contributor
e14 Contributor over 10 years ago

Hello, I would like to use a share data cache (L2) between the PS and one custom IP.

I used the System Cache IP, connected to M_GP0.
The L2 cache should be placed before the DDR memory.

The architecture of the system is available here : http://img15.hostingpics.net/pics/171358architecture.png

The memory mapping is available here :
http://img15.hostingpics.net/pics/611571memorymapping.png

After looking with the ILA, no data is present on the while debugging with SDK

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I could not understand your architecture's picture: the PS is directly connected to an external DDR, and you say that it should be placed after the "System Cache IP"...

    Maybe you think on a Microblaze, instead of the PS, connected to the system_cache_0 through the axi_interconnect_0.

    In addition, you say that no data is present in the ILA while debugging with SDK. Is the complete system working without the ILA?

    I would suggest to try first a simple memory, instead of a custom IP.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I could not understand your architecture's picture: the PS is directly connected to an external DDR, and you say that it should be placed after the "System Cache IP"...

    Maybe you think on a Microblaze, instead of the PS, connected to the system_cache_0 through the axi_interconnect_0.

    In addition, you say that no data is present in the ILA while debugging with SDK. Is the complete system working without the ILA?

    I would suggest to try first a simple memory, instead of a custom IP.