Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Errata: USB Host cap slightly out-of-spec
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 489 views
  • Users 0 members are here
Related

Errata: USB Host cap slightly out-of-spec

bhfletcher
bhfletcher over 13 years ago

Please be aware that we are slightly out-of-spec on a capacitor that is required to put the TUSB1210 USB PHY into Host mode.  C89 correctly shows as 120uF in the schematic.  However, 100uF is populated.  I don’t expect this to be a problem, but it is a possibility.  Those concerned with meeting this specification should change out C89 for 120uF.  Here is an explanation from TI Engineering regarding the possible implications:

USB2.0 OTG2.0 spec max ext cap on VBUS is 6.5uF on Host side and 6.5uF on Device side (13uF total). Host only application requires > 120uF (CHPB in USB2.0 Table7-7).

OTG2.0 ADP (and OTG1.3 VBUS pulsing) make use of the differences in VBUS capacitances for detections.

So you must provide the VBUS capacitance according to the target specification.

 

I will be publishing an errata to this effect shortly.

 

Bryan

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    I thought of 3 more that I will also add to the document.

    1.   Since the ZedBoard uses ES silicon, the Zynq errata affects ZedBoard.  Everyone should read and understand the errata affecting the 7Z020.
    2.   DDR3 CKE is now recommended to be pulled up through 40-ohms to VTT.  We have not seen any failures related to this.
    3.   SD_CLK is now recommended to be terminated with a 40 to 60-ohm series resistor.  We have not seen any failures related to this.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    I thought of 3 more that I will also add to the document.

    1.   Since the ZedBoard uses ES silicon, the Zynq errata affects ZedBoard.  Everyone should read and understand the errata affecting the 7Z020.
    2.   DDR3 CKE is now recommended to be pulled up through 40-ohms to VTT.  We have not seen any failures related to this.
    3.   SD_CLK is now recommended to be terminated with a 40 to 60-ohm series resistor.  We have not seen any failures related to this.

    Bryan