Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Understanding Ethernet on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 7377 views
  • Users 0 members are here
Related

Understanding Ethernet on Zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi Everyone!



I am  not very experienced with the Zedboard and having a ruff time understanding the infrastructure around the Ethernet functionality on the Zedboard.



I have read the related chapters in the following documents, but so far I was not able to put it all together.



1 Zedboard HW User Guide Version 1.1
2 UG585 (v1.10) February 23, 2015
3 various posts such as:
http://zedboard.org/content/redirecting-peripherals-mio-emio



So, as far as I understand there is a Marvell Ethernet PHY on the Zedboard which is directly connected to the PS's MIO Bank 1(via RGMII). Further more, there are two Ethernet MACs in the Processing System which are also connected to the MIO Bank via RGMII(over a GMII/RGMII adapter). Additionally, these two Ethernet MACs are connected to the Zedboards DDR3 RAM via a DMA Controller.



Question A:
Is that correct? Did I miss something important?



One of my goals is to get Ethernet frames/packets into the PL where I want to build some logic to analyse Headers etc.. (proof of concept / educational work)




Similar to Link 3 I redirected eth0 to EMIO(I am working with Vivado btw) and got a MDIO and a GMII Port added to my Processing System block view.




Question B:
Where exactly are these interfaces(GMII and MDIO) connected to? I think to one of the Ethernet MACs of the PS?!




Question(s) C:
What do I have to do now in order to get Ethernet packets to my custom IP?
Do I have to initialize the Ethernet MAC of the PS using DMA(from one of the arm cores) like described in 2 and get packets from RAM to my IP?
Or is there a way to get packets over the above mentioned GMII?
Or is it possible to get a direct connection to the Marvell PHY?




kind regards and a big thank you in advance!

PS:Sorry for the bad formatting.. I added blank lines but paragraphs are not recognized appropriately 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The Zynq PS based Ethernet MAC and associated DMA controller are internal to the Processing System and not on the AXI bus.

     

    Take a look at the Zynq Technical Reference Manual, Chapter 16 for details:

     http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The Zynq PS based Ethernet MAC and associated DMA controller are internal to the Processing System and not on the AXI bus.

     

    Take a look at the Zynq Technical Reference Manual, Chapter 16 for details:

     http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bbgator
    0 bbgator over 9 years ago in reply to e14 Contributor
    This looks exactly what he wants.   The code is already done
     
    Zynq-7000 AP SoC - Bare Metal - Redirecting Packets to PL Tech Tip

    http://www.wiki.xilinx.com/Zynq-7000+AP+SoC+-+Performance+-+Ethernet+Packet+Inspection+-+Bare+Metal+-+Redirecting++Packets+to+PL+Tech+Tip