Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Assigning Pins to a Custom Peripheral
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 1110 views
  • Users 0 members are here
Related

Assigning Pins to a Custom Peripheral

chipslinger
chipslinger over 13 years ago

I'm trying to bring out pins from a custom peripheral, but they're not showing up in the pinout report.

What I did was take the generated register set, add in new i/o signals, new logic, and new components that are in separate files. So, what was once a register set, is now a series of peripherals, like SPI controllers, i/o ports, timers, etc...

I can write/read the registers from a simple diagnostic program, so my hardware seems to actually exist.

When I first created the register set, the only connections were to the AXI bus. There are now about 40 lines that I need to assign to pins.

I've added the file names to the .PRJ and .PAO files. I've figured out that I need to (eventually) add the pin names to the data<project>.ucf file, but right now the pin names don't show up in the pin report, so I get an error if I add them into the ucf file.

How do I make the pins (which are now at the top level of the register set) show up as pins on the device?

  • Sign in to reply
  • Cancel
Parents
  • chipslinger
    0 chipslinger over 13 years ago

    I'm pretty sure that I'm doing exactly what you say is necessary. However, the pins don't show up on the part after compilation. I used the IP interface wizard to create a register bank. The two files created are:
      - bus_interface.vhd (top level IP file)
      - user_logic.vhd
    I have the ports on bus_interface.vhd. Some connect through to user_logic.vhd, some refer to logic in bus_interface.vhd
    I added the ports to the MPD file.
    I rescanned the user repository
    I see the ports within XPS and have selected MAKE EXTERNAL.
    I can see the ports in the part instantiation template.

    I have simulated the design in modelsim, so I'm pretty sure that the logic isn't being munched away b/c of a design error.

    The ports do not show as external pins in the pinout file, though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chipslinger
    0 chipslinger over 13 years ago

    I'm pretty sure that I'm doing exactly what you say is necessary. However, the pins don't show up on the part after compilation. I used the IP interface wizard to create a register bank. The two files created are:
      - bus_interface.vhd (top level IP file)
      - user_logic.vhd
    I have the ports on bus_interface.vhd. Some connect through to user_logic.vhd, some refer to logic in bus_interface.vhd
    I added the ports to the MPD file.
    I rescanned the user repository
    I see the ports within XPS and have selected MAKE EXTERNAL.
    I can see the ports in the part instantiation template.

    I have simulated the design in modelsim, so I'm pretty sure that the logic isn't being munched away b/c of a design error.

    The ports do not show as external pins in the pinout file, though.