Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Assigning Pins to a Custom Peripheral
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 361 subscribers
  • Views 1111 views
  • Users 0 members are here
Related

Assigning Pins to a Custom Peripheral

chipslinger
chipslinger over 13 years ago

I'm trying to bring out pins from a custom peripheral, but they're not showing up in the pinout report.

What I did was take the generated register set, add in new i/o signals, new logic, and new components that are in separate files. So, what was once a register set, is now a series of peripherals, like SPI controllers, i/o ports, timers, etc...

I can write/read the registers from a simple diagnostic program, so my hardware seems to actually exist.

When I first created the register set, the only connections were to the AXI bus. There are now about 40 lines that I need to assign to pins.

I've added the file names to the .PRJ and .PAO files. I've figured out that I need to (eventually) add the pin names to the data<project>.ucf file, but right now the pin names don't show up in the pin report, so I get an error if I add them into the ucf file.

How do I make the pins (which are now at the top level of the register set) show up as pins on the device?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    If you right-click on the .xmp file in PlanAhead and select "View Instantiation Template" do the pins show up in the HDL code?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    If you right-click on the .xmp file in PlanAhead and select "View Instantiation Template" do the pins show up in the HDL code?