Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design RS485 wit AXI UARTLITE
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1135 views
  • Users 0 members are here
Related

RS485 wit AXI UARTLITE

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I managed to use tty for rs232 via axi_uartlite and connected r232 pmod.

Now i wanted to use the rs485 PMOD via Linux on the Zedboard.

Therefore i wrote an IP-Core for setting DE / !RO.

My solution is to keep DE HIGH as long as the a LOW is written over TX. A Timer will keep DE High for at least WORD transmitted (let's say 10 Bytes) and will go LOW afterwards. Everytime a new LOW is written to TX the Counter will restart.

Via linux i can use the AXI-UARTLITE and send commands via tty but i cant receive them, only random ascii characters...

With a Scope i checked the DE signal and it works fine, but when i'm trying to read data it doenst work. But after a while it is possible to send data from pc to the pmod and read them via tty but then it's not possbile to send data via pmod... i hope you understood my problem.

Is there anything i have to think about?

I appreciate every help :)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

     

    It could be a lot of things. First, you might want to instrument both the DE and TX/RX signals to see the relationship.

     

    What protocol and transfer speed are you using?

    How long does the receiving unit on the other end expect the first 'low' to be?

    Does the delay from your IP detecting the low to asserting the DE signal truncate the signal too much?

    Does your timer that extends the DE signal assertion distort the signal received by the receiving node? ( would it make your Stop bit too long)

    How long does the other node wait before asserting a return message. Could the DE signal still be asserted and interfering with the data from the other end?

     

    Again, I would suggest instrumenting the data signals and comparing the results to your protocol and expected data.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary!

    Thanks for your reply.

    Do you mean, that i should check the scope signals with my expected protocol? I already did this, but it looks for me, that in the moment of receiving data, the Driver on the PMOD tries to set the DE High.

    I'm sending Data via a USB to RS485 Adapter to the PMOD RS485 attached to the Zedboard and from one PMOD to another PMOD, but it ends with the same results.

    Maybe you're right, that i extend the Stop bit too much, is there any document or so with some specs about the signal length of the DE signal?

    Tahnks

    Wahid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    The Protocoll is 8N1 with 56700 Baudrate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Wahid,

     

    Our expertise is focused on the Zynq based 'zed boards. You will need to research RS485 specs and advice in another venue.

     

    -Gary