Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design RS485 wit AXI UARTLITE
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1145 views
  • Users 0 members are here
Related

RS485 wit AXI UARTLITE

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I managed to use tty for rs232 via axi_uartlite and connected r232 pmod.

Now i wanted to use the rs485 PMOD via Linux on the Zedboard.

Therefore i wrote an IP-Core for setting DE / !RO.

My solution is to keep DE HIGH as long as the a LOW is written over TX. A Timer will keep DE High for at least WORD transmitted (let's say 10 Bytes) and will go LOW afterwards. Everytime a new LOW is written to TX the Counter will restart.

Via linux i can use the AXI-UARTLITE and send commands via tty but i cant receive them, only random ascii characters...

With a Scope i checked the DE signal and it works fine, but when i'm trying to read data it doenst work. But after a while it is possible to send data from pc to the pmod and read them via tty but then it's not possbile to send data via pmod... i hope you understood my problem.

Is there anything i have to think about?

I appreciate every help :)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary!

    Thanks for your reply.

    Do you mean, that i should check the scope signals with my expected protocol? I already did this, but it looks for me, that in the moment of receiving data, the Driver on the PMOD tries to set the DE High.

    I'm sending Data via a USB to RS485 Adapter to the PMOD RS485 attached to the Zedboard and from one PMOD to another PMOD, but it ends with the same results.

    Maybe you're right, that i extend the Stop bit too much, is there any document or so with some specs about the signal length of the DE signal?

    Tahnks

    Wahid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary!

    Thanks for your reply.

    Do you mean, that i should check the scope signals with my expected protocol? I already did this, but it looks for me, that in the moment of receiving data, the Driver on the PMOD tries to set the DE High.

    I'm sending Data via a USB to RS485 Adapter to the PMOD RS485 attached to the Zedboard and from one PMOD to another PMOD, but it ends with the same results.

    Maybe you're right, that i extend the Stop bit too much, is there any document or so with some specs about the signal length of the DE signal?

    Tahnks

    Wahid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    The Protocoll is 8N1 with 56700 Baudrate