Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Video Chain Establishment using Xilinx Zynq 7Z020 ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 687 views
  • Users 0 members are here
Related

Video Chain Establishment using Xilinx Zynq 7Z020 ?

e14 Contributor
e14 Contributor over 12 years ago


Hi all,

I want to establish a video chain using Zed Board and develop a video processing algorithm on it. Our university recently purchased a Zed Board of XC7z020-CLG484-1 . But it is not a Video Imaging Kit of Zed Board. That's a challenge i have been facing.

Is it possible to establish a video chain on the Zed board of xilinx zynq 7Z020? If yes, then what are the extra resources required to this Zedboard.
Kindly help me regarding this.

Thank you.
With Regards,
Sofia Nayak.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Sofia,

    It sounds like you could do with a bit of inspiration - how's this for an idea?

    Hack open a HDMI cable, connect up to the Differential PMOD inputs on the Zedboard (careful with that 5V wire - it will fry your Zynq!).

    If the gods are shining on you, and you have 50 Ohm resistors pulling to 3.3V on the input as required by (see "Xilinx UG471 7 Series FPGAs SelectIO Resources User Guide") , you may be able to receive TMDS input (aka DVI-D) without any extra hardware. Have a look at the Digilent Atlys board schematics for ideas.

    You should then be able to connect to a suitable source (e.g. a laptop). You might also need to implement an EDID EEPROM to allow the source to decide what format to send. Look at "Extended display identification data" on Wikipedia.

    You might be limited to 720p (1280x720) due to the input SERDES topping out at 1250Mb/s.

    As a test you could see if you can recover the TMDS clock. I would strongly suggest you use another FPGA board to generate a TMDS source signal that you can experiment with without needing a fully featured DVI-D input interface. This should quickly let you know if you can reliably receive TDMS at the 750Mb/s per channel needed to support 720p.

    The often-referred-to XAPP495 will give you plenty of guidance.

    You will also want to give this paper a good read - dvi_spec-V1_0.pdf - just Google for it

    So the video chain could be....

    Laptop - HDMI cable (running as DVI-D) - Zynq PMOD - PL logic - Zedboard's ADV7511 - Monitor

    If you like you can use my DVI-D output design from my site (google "Zedboard VGA HDMI") to do the last couple of hops of the chain.

    Hope it helps - if you want you can email me (hamster at snap dot net dot nz).

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Sofia,

    It sounds like you could do with a bit of inspiration - how's this for an idea?

    Hack open a HDMI cable, connect up to the Differential PMOD inputs on the Zedboard (careful with that 5V wire - it will fry your Zynq!).

    If the gods are shining on you, and you have 50 Ohm resistors pulling to 3.3V on the input as required by (see "Xilinx UG471 7 Series FPGAs SelectIO Resources User Guide") , you may be able to receive TMDS input (aka DVI-D) without any extra hardware. Have a look at the Digilent Atlys board schematics for ideas.

    You should then be able to connect to a suitable source (e.g. a laptop). You might also need to implement an EDID EEPROM to allow the source to decide what format to send. Look at "Extended display identification data" on Wikipedia.

    You might be limited to 720p (1280x720) due to the input SERDES topping out at 1250Mb/s.

    As a test you could see if you can recover the TMDS clock. I would strongly suggest you use another FPGA board to generate a TMDS source signal that you can experiment with without needing a fully featured DVI-D input interface. This should quickly let you know if you can reliably receive TDMS at the 750Mb/s per channel needed to support 720p.

    The often-referred-to XAPP495 will give you plenty of guidance.

    You will also want to give this paper a good read - dvi_spec-V1_0.pdf - just Google for it

    So the video chain could be....

    Laptop - HDMI cable (running as DVI-D) - Zynq PMOD - PL logic - Zedboard's ADV7511 - Monitor

    If you like you can use my DVI-D output design from my site (google "Zedboard VGA HDMI") to do the last couple of hops of the chain.

    Hope it helps - if you want you can email me (hamster at snap dot net dot nz).

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you for your quick response and valuable suggestion. I must go through it while working.

    Ya, I am planning to establish video signal chain using Zedboard 7Z020 which is not a video imaging kit.But it has a LPC FMC connector. That's why i think FMC module provided by Avnet will work with this 7Z020 board.
    Because i am a beginner to use this board.
    That's why i am interested to know,is anybody work with this 7Z020 board for video image processing?
    If yes,then how?Please provide few references.
    Thank you.
    Regards
    Sofia.