Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Is ZedBoard SD reader compatible with ultra high speed SD cards?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 647 views
  • Users 0 members are here
Related

Is ZedBoard SD reader compatible with ultra high speed SD cards?

e14 Contributor
e14 Contributor over 12 years ago

I would like to know if the Zedboard SD reader is compatible with the SD cards new generation, the ultra high speed SD cards. I also would like to know if there could be performance benefits. Thanks a lot.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I am using SD card that's marked with "UHS Speed Class 1" and "class 10" with Zedboard.  The SD card boots up significantly faster than regular SD cards. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I'm also using 32GB SanDisk UHS Speed Class 1 (U1) card without any problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brendansimon
    0 brendansimon over 10 years ago

    Which 32GB SanDisk card did you use that worked?

    I've tried Sandisk Ultra UHS-1 32GB MicroSD (with adapter) and the linux kernel hung during boot - before even trying to mount the rootfs.

    My Sandisk Ultra UHS-1 16GB MicroSD card fails the same way.

    My Sandisk Ultra UHS-1 8GB MicroSD card works fine.

    Why does the 8GB work?  Did I just get lucky?
    Why does 32GB fail (same brand, type, etc) ?

    I tried a 16GB Samsung EVO UHS-1 and that worked.  I will try a Samsung 32GB EVO soon.

    However, I don't feel confident with all this.  Is it just pot luck?  Surely there must be some spec that says these types of cards should or shouldn't work.

    Any help greatly appreciated.