Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Linaro problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 361 subscribers
  • Views 740 views
  • Users 0 members are here
Related

Linaro problem

e14 Contributor
e14 Contributor over 11 years ago

Hi, i have followed this tutorial:
http://www.digilentinc.com/Data/Products/EMBEDDED-LINUX/ZedBoard_GSwEL_Guide.pdf


the ramdisk file system works great, but whe i do the appropriate change for the linaro file system the serial port output this:

____________________________________________________________
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading zImage

2479640 bytes read
reading devicetree.dtb

9652 bytes read
reading ramdisk8M.image.gz

** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #2 SMP PREEMPT Thu Jul 12 21:01:
42 PDT 2012
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
[    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
[    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
[    0.000000] PERCPU: Embedded 7 pages/cpu @c0926000 s5696 r8192 d14784 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=1
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 240MB 256MB = 496MB total
[    0.000000] Memory: 498040k/498040k available, 26248k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)
[    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)
[    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)
[    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Verbose stalled-CPUs detection is disabled.
[    0.000000] NR_IRQS:128
[    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.000000] Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
[    0.090000] pid_max: default: 32768 minimum: 301
[    0.090000] Mount-cache hash table entries: 512
[    0.090000] CPU: Testing write buffer coherency: ok
[    0.100000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.100000] smp_twd: clock not found: -2
[    0.110000] Calibrating local timer... 333.56MHz.
[    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c
[    0.270000] CPU1: Booted secondary processor
[    0.360000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.360000] Brought up 2 CPUs
[    0.360000] SMP: Total of 2 processors activated (2664.03 BogoMIPS).
[    0.370000] devtmpfs: initialized
[    0.370000] ------------[ cut here ]------------
[    0.380000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.380000] Modules linked in:
[    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.420000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.440000] ---[ end trace 1b75b31a2719ed1c ]---
[    0.450000] ------------[ cut here ]------------
[    0.450000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.460000] Modules linked in:
[    0.460000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.470000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.480000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.490000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.500000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.510000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.520000] ---[ end trace 1b75b31a2719ed1d ]---
[    0.520000] NET: Registered protocol family 16
[    0.540000] L310 cache controller enabled
[    0.540000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B
[    0.550000] registering platform device 'pl330' id 0
[    0.550000] registering platform device 'arm-pmu' id 0
[    0.560000]
[    0.560000] ###############################################
[    0.560000] #                                             #
[    0.570000] #                Board ZED Init               #
[    0.570000] #                                             #
[    0.580000] ###############################################
[    0.580000]
[    0.590000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.590000] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.620000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000
[    0.640000] bio: create slab <bio-0> at 0
[    0.640000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops
[    0.640000] xgpiops e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe080a000
[    0.650000] SCSI subsystem initialized
[    0.660000] usbcore: registered new interface driver usbfs
[    0.660000] usbcore: registered new interface driver hub
[    0.670000] usbcore: registered new device driver usb
[    0.670000] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.680000] Switching to clocksource xttcpss_timer1
[    0.690000] NET: Registered protocol family 2
[    0.690000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.700000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    0.700000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)
[    0.710000] TCP: Hash tables configured (established 16384 bind 16384)
[    0.720000] TCP reno registered
[    0.720000] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.730000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.730000] NET: Registered protocol family 1
[    0.740000] xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400
[    0.740000] pl330 dev 0 probe success
[    0.750000] msgmni has been set to 972
[    0.750000] io scheduler noop registered
[    0.750000] io scheduler deadline registered
[    0.760000] io scheduler cfq registered (default)
[    0.760000] e00010[    0.770000] console [ttyPS0] enabled, bootconsole disabled
[    0.770000] console [ttyPS0] enabled, bootconsole disabled
[    0.780000] xdevcfg f8007000.ps7-dev-cfg: ioremap f8007000 to e0810000 with size 1000
[    0.790000] [drm] Initialized drm 1.1.0 20060810
[    0.800000] brd: module loaded
[    0.810000] loop: module loaded
[    0.820000] xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xE0812000, irq=51
[    0.830000] GEM: BASEADDRESS hw: e000b000 virt: e0814000
[    0.830000] XEMACPS mii bus: probed
[    0.840000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
[    0.840000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.850000] usb_hcd_xusbps_probe: No OTG assigned!
[    0.850000] usb_hcd_xusbps_probe: OTG now assigned!
[    0.860000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    0.870000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    0.900000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    0.920000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    0.920000] hub 1-0:1.0: USB hub found
[    0.930000] hub 1-0:1.0: 1 port detected
[    0.930000] Initializing USB Mass Storage driver...
[    0.930000] usbcore: registered new interface driver usb-storage
[    0.940000] USB Mass Storage support registered.
[    0.950000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
[    0.950000] mousedev: PS/2 mouse device common for all mice
[    0.960000] Linux video capture interface: v2.00
[    0.960000] gspca_main: v2.14.0 registered
[    0.970000] usbcore: registered new interface driver uvcvideo
[    0.970000] USB Video Class driver (1.1.1)
[    0.980000] sdhci: Secure Digital Host Controller Interface driver
[    0.980000] sdhci: Copyright(c) Pierre Ossman
[    0.990000] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.000000] usbcore: registered new interface driver usbhid
[    1.000000] usbhid: USB HID core driver
[    1.010000] adv7511 0-0039: Failed to add route DAI IN->TMDS
[    1.020000] edid status: 41
[    1.030000] asoc: adv7511 <-> 75c00000.axi-spdif-tx mapping ok
[    1.030000] axi-spdif 75c00000.axi-spdif-tx: Failed to set DAI format: -22
[    1.040000] ALSA device list:
[    1.040000]   #0: HDMI monitor
[    1.050000] TCP cubic registered
[    1.050000] NET: Registered protocol family 17
[    1.060000] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    1.060000] Registering SWP/SWPB emulation handler
[    1.070000] registered taskstats version 1
[    1.070000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    1.080000] Waiting for root device /dev/mmcblk0p2...
[    1.380000] edid ret: 0
[    1.380000] new mode: 640x480 800x525 25175
[    1.380000] new mode: 800x600 1024x625 36000
[    1.390000] new mode: 800x600 1056x628 40000
[    1.390000] new mode: 848x480 1088x517 33750
[    1.390000] new mode: 1024x768 1344x806 65000
[    1.400000] drivers/gpu/drm/analog/analog_drm_fbdev.c:analog_drm_fbdev_probe[241]
[    1.420000] setting clock to: 65000
[    1.420000] raw_edid:   (null) 0
[    1.420000] Using RGB output
[    1.450000] Console: switching to colour frame buffer device 128x48
[    1.480000] fb0:  frame buffer device
[    1.480000] drm: registered panic notifier
[    1.480000] [drm] Initialized analog_drm 1.0.0 20110530 on minor 0
____________________________________________________________

and on the HDMI screen two tux image appear in the upper-left corner, furtherlly if i attach an usb mouse to the OTG port it doesn't light up. What's the problem?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The thing that leaps out at me in your log is that uboot is unable to correctly copy the ramdisk to non-volatile memory.   I think resolving the reason for that error is the key to getting your system to boot correctly to the command prompt.  Could be a simple as using a different SD card.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    thanks for the reply, now the file names are correct, but u-boot keep stucking at PS/2 mouse device:

    Copying Linux from SD to RAM...
    Unknown command
    Unknown command
    Device: SDHCI
    Manufacturer ID: 27
    OEM: 5048
    Name: SD04G
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 1.10
    High Capacity: Yes
    Capacity: 3980394496
    Bus Width: 1-bit
    reading zImage

    2362848 bytes read
    reading devicetree.dtb

    9648 bytes read
    reading ramdisk8M.image.gz

    3694108 bytes read
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Booting Linux on physical CPU 0
    [    0.000000] Linux version 3.6.0-digilent-13.01-00002-g06b3889-dirty (luca@NeuroneLab) (gcc version 4.8.3 20140320 (prerelease) (Sourcery CodeBench Lite 2014.05-23) ) #3 SMP PREEMPT Mon Nov 3 18:27:09 CET 2014
    [    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
    [    0.000000] Memory policy: ECC disabled, Data cache writealloc
    [    0.000000] PERCPU: Embedded 7 pages/cpu @c140a000 s6976 r8192 d13504 u32768
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048
    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootwait devtmpfs.mount=1
    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Memory: 512MB = 512MB total
    [    0.000000] Memory: 506756k/506756k available, 17532k reserved, 0K highmem
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    [    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc0424cac   (4212 kB)
    [    0.000000]       .init : 0xc0425000 - 0xc044ab40   ( 151 kB)
    [    0.000000]       .data : 0xc044c000 - 0xc04849a0   ( 227 kB)
    [    0.000000]        .bss : 0xc04849c4 - 0xc049b130   (  90 kB)
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Dump stacks of tasks blocking RCU-preempt GP.
    [    0.000000]  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    [    0.000000] NR_IRQS:512
    [    0.000000] Zynq clock init
    [    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
    [    0.000000] sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms
    [    0.000000] Console: colour dummy device 80x30
    [    0.090000] Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
    [    0.090000] pid_max: default: 32768 minimum: 301
    [    0.090000] Mount-cache hash table entries: 512
    [    0.090000] CPU: Testing write buffer coherency: ok
    [    0.090000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.090000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
    [    0.090000] Setting up static identity map for 0x2f1088 - 0x2f10bc
    [    0.090000] L310 cache controller enabled
    [    0.090000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B
    [    0.130000] Map SLCR registers
    [    0.130000] CPU1: Booted secondary processor
    [    0.220000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.220000] Brought up 2 CPUs
    [    0.220000] SMP: Total of 2 processors activated (2664.03 BogoMIPS).
    [    0.220000] devtmpfs: initialized
    [    0.220000] NET: Registered protocol family 16
    [    0.220000] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.220000] xgpiops e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe084a000
    [    0.230000] registering platform device 'pl330' id 0
    [    0.230000] registering platform device 'arm-pmu' id 0
    [    0.230000] registering platform device 'zynq-dvfs' id 0
    [    0.230000]
    [    0.230000] ###############################################
    [    0.230000] #                                             #
    [    0.230000] #                Board ZED Init               #
    [    0.230000] #                                             #
    [    0.230000] ###############################################
    [    0.230000]
    [    0.230000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    [    0.230000] hw-breakpoint: maximum watchpoint size is 4 bytes.
    [    0.250000] xslcr xslcr.0: at 0xF8000000 mapped to 0xF8000000
    [    0.260000] bio: create slab <bio-0> at 0
    [    0.270000] SCSI subsystem initialized
    [    0.270000] usbcore: registered new interface driver usbfs
    [    0.270000] usbcore: registered new interface driver hub
    [    0.270000] usbcore: registered new device driver usb
    [    0.270000] Advanced Linux Sound Architecture Driver Version 1.0.25.
    [    0.270000] Switching to clocksource xttcpss_timer1
    [    0.280000] NET: Registered protocol family 2
    [    0.280000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
    [    0.280000] TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
    [    0.280000] TCP: Hash tables configured (established 16384 bind 16384)
    [    0.280000] TCP: reno registered
    [    0.280000] UDP hash table entries: 256 (order: 1, 8192 bytes)
    [    0.280000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    [    0.280000] NET: Registered protocol family 1
    [    0.280000] Trying to unpack rootfs image as initramfs...
    [    0.280000] rootfs image is not initramfs (no cpio magic); looks like an initrd
    [    0.310000] Freeing initrd memory: 8192K
    [    0.320000] pl330 dev 0 probe success
    [    0.320000] msgmni has been set to 1005
    [    0.320000] io scheduler noop registered
    [    0.320000] io scheduler deadline registered
    [    0.320000] io scheduler cfq registered (default)
    [    0.320000] e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 82) is a xuartps
    [    0.810000] console [ttyPS0] enabled
    [    0.820000] xdevcfg f8007000.ps7-dev-cfg: ioremap f8007000 to e0850000 with size 1000
    [    0.820000] [drm] Initialized drm 1.1.0 20060810                                                                                  
    [    0.840000] brd: module loaded                                                                                                    
    [    0.850000] loop: module loaded                                                                                                   
    [    0.850000] xqspips e000d000.ps7-qspi: master is unqueued, this is deprecated                                                     
    [    0.860000] xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xE0852000, irq=51                                                 
    [    0.870000] libphy: XEMACPS mii bus: probed
    [    0.870000] xemacps e000b000.ps7-ethernet: pdev->id -1, baseaddr 0xe000b000, irq 54
    [    0.880000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    0.890000] usb_hcd_xusbps_probe: No OTG assigned!
    [    0.890000] usb_hcd_xusbps_probe: OTG now assigned!
    [    0.900000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
    [    0.910000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
    [    0.940000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
    [    0.960000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
    [    0.960000] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    0.970000] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    0.980000] usb usb1: Product: Xilinx PS USB EHCI Host Controller
    [    0.980000] usb usb1: Manufacturer: Linux 3.6.0-digilent-13.01-00002-g06b3889-dirty ehci_hcd
    [    0.990000] usb usb1: SerialNumber: xusbps-ehci.0
    [    0.990000] hub 1-0:1.0: USB hub found
    [    1.000000] hub 1-0:1.0: 1 port detected
    [    1.000000] Initializing USB Mass Storage driver...
    [    1.010000] usbcore: registered new interface driver usb-storage
    [    1.010000] USB Mass Storage support registered.
    [    1.020000] mousedev: PS/2 mouse device common for all mice

    this does not happens when i use the default bitstream, it happens only when i use mine, where is the error now?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    Have you checked your device tree?  The chances are that some hardware which is available in the default bitstream can't be found in your hardware design which is causing a driver to fail (for example the OLED screen).  There's a good tutorial for this here:

    http://xillybus.com/tutorials/device-tree-zynq-1

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    thanks for the reply, now it seems working, but when i do
        insmod myled.ko
    nothing happen, in proc directory the myled file doesn't appear, but if i do lsmod the myled module is correctly loaded, could it be a device tree problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Hi 

    how do you solve the problem of keeping stucking at PS/2 mouse device?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi,

    Please ask your question over at Digilent as it is referenced to their material.

    Thank you,

    Josh