Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Linaro problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 361 subscribers
  • Views 738 views
  • Users 0 members are here
Related

Linaro problem

e14 Contributor
e14 Contributor over 11 years ago

Hi, i have followed this tutorial:
http://www.digilentinc.com/Data/Products/EMBEDDED-LINUX/ZedBoard_GSwEL_Guide.pdf


the ramdisk file system works great, but whe i do the appropriate change for the linaro file system the serial port output this:

____________________________________________________________
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading zImage

2479640 bytes read
reading devicetree.dtb

9652 bytes read
reading ramdisk8M.image.gz

** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #2 SMP PREEMPT Thu Jul 12 21:01:
42 PDT 2012
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
[    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
[    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
[    0.000000] PERCPU: Embedded 7 pages/cpu @c0926000 s5696 r8192 d14784 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824
[    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=1
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 240MB 256MB = 496MB total
[    0.000000] Memory: 498040k/498040k available, 26248k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)
[    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)
[    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)
[    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Verbose stalled-CPUs detection is disabled.
[    0.000000] NR_IRQS:128
[    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.000000] Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
[    0.090000] pid_max: default: 32768 minimum: 301
[    0.090000] Mount-cache hash table entries: 512
[    0.090000] CPU: Testing write buffer coherency: ok
[    0.100000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.100000] smp_twd: clock not found: -2
[    0.110000] Calibrating local timer... 333.56MHz.
[    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
[    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c
[    0.270000] CPU1: Booted secondary processor
[    0.360000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.360000] Brought up 2 CPUs
[    0.360000] SMP: Total of 2 processors activated (2664.03 BogoMIPS).
[    0.370000] devtmpfs: initialized
[    0.370000] ------------[ cut here ]------------
[    0.380000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.380000] Modules linked in:
[    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.420000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.440000] ---[ end trace 1b75b31a2719ed1c ]---
[    0.450000] ------------[ cut here ]------------
[    0.450000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()
[    0.460000] Modules linked in:
[    0.460000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)
[    0.470000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)
[    0.480000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)
[    0.490000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)
[    0.500000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)
[    0.510000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)
[    0.520000] ---[ end trace 1b75b31a2719ed1d ]---
[    0.520000] NET: Registered protocol family 16
[    0.540000] L310 cache controller enabled
[    0.540000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B
[    0.550000] registering platform device 'pl330' id 0
[    0.550000] registering platform device 'arm-pmu' id 0
[    0.560000]
[    0.560000] ###############################################
[    0.560000] #                                             #
[    0.570000] #                Board ZED Init               #
[    0.570000] #                                             #
[    0.580000] ###############################################
[    0.580000]
[    0.590000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.590000] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.620000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000
[    0.640000] bio: create slab <bio-0> at 0
[    0.640000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops
[    0.640000] xgpiops e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe080a000
[    0.650000] SCSI subsystem initialized
[    0.660000] usbcore: registered new interface driver usbfs
[    0.660000] usbcore: registered new interface driver hub
[    0.670000] usbcore: registered new device driver usb
[    0.670000] Advanced Linux Sound Architecture Driver Version 1.0.24.
[    0.680000] Switching to clocksource xttcpss_timer1
[    0.690000] NET: Registered protocol family 2
[    0.690000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[    0.700000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[    0.700000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)
[    0.710000] TCP: Hash tables configured (established 16384 bind 16384)
[    0.720000] TCP reno registered
[    0.720000] UDP hash table entries: 256 (order: 1, 8192 bytes)
[    0.730000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[    0.730000] NET: Registered protocol family 1
[    0.740000] xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400
[    0.740000] pl330 dev 0 probe success
[    0.750000] msgmni has been set to 972
[    0.750000] io scheduler noop registered
[    0.750000] io scheduler deadline registered
[    0.760000] io scheduler cfq registered (default)
[    0.760000] e00010[    0.770000] console [ttyPS0] enabled, bootconsole disabled
[    0.770000] console [ttyPS0] enabled, bootconsole disabled
[    0.780000] xdevcfg f8007000.ps7-dev-cfg: ioremap f8007000 to e0810000 with size 1000
[    0.790000] [drm] Initialized drm 1.1.0 20060810
[    0.800000] brd: module loaded
[    0.810000] loop: module loaded
[    0.820000] xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xE0812000, irq=51
[    0.830000] GEM: BASEADDRESS hw: e000b000 virt: e0814000
[    0.830000] XEMACPS mii bus: probed
[    0.840000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
[    0.840000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    0.850000] usb_hcd_xusbps_probe: No OTG assigned!
[    0.850000] usb_hcd_xusbps_probe: OTG now assigned!
[    0.860000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
[    0.870000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
[    0.900000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
[    0.920000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
[    0.920000] hub 1-0:1.0: USB hub found
[    0.930000] hub 1-0:1.0: 1 port detected
[    0.930000] Initializing USB Mass Storage driver...
[    0.930000] usbcore: registered new interface driver usb-storage
[    0.940000] USB Mass Storage support registered.
[    0.950000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
[    0.950000] mousedev: PS/2 mouse device common for all mice
[    0.960000] Linux video capture interface: v2.00
[    0.960000] gspca_main: v2.14.0 registered
[    0.970000] usbcore: registered new interface driver uvcvideo
[    0.970000] USB Video Class driver (1.1.1)
[    0.980000] sdhci: Secure Digital Host Controller Interface driver
[    0.980000] sdhci: Copyright(c) Pierre Ossman
[    0.990000] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.000000] usbcore: registered new interface driver usbhid
[    1.000000] usbhid: USB HID core driver
[    1.010000] adv7511 0-0039: Failed to add route DAI IN->TMDS
[    1.020000] edid status: 41
[    1.030000] asoc: adv7511 <-> 75c00000.axi-spdif-tx mapping ok
[    1.030000] axi-spdif 75c00000.axi-spdif-tx: Failed to set DAI format: -22
[    1.040000] ALSA device list:
[    1.040000]   #0: HDMI monitor
[    1.050000] TCP cubic registered
[    1.050000] NET: Registered protocol family 17
[    1.060000] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    1.060000] Registering SWP/SWPB emulation handler
[    1.070000] registered taskstats version 1
[    1.070000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[    1.080000] Waiting for root device /dev/mmcblk0p2...
[    1.380000] edid ret: 0
[    1.380000] new mode: 640x480 800x525 25175
[    1.380000] new mode: 800x600 1024x625 36000
[    1.390000] new mode: 800x600 1056x628 40000
[    1.390000] new mode: 848x480 1088x517 33750
[    1.390000] new mode: 1024x768 1344x806 65000
[    1.400000] drivers/gpu/drm/analog/analog_drm_fbdev.c:analog_drm_fbdev_probe[241]
[    1.420000] setting clock to: 65000
[    1.420000] raw_edid:   (null) 0
[    1.420000] Using RGB output
[    1.450000] Console: switching to colour frame buffer device 128x48
[    1.480000] fb0:  frame buffer device
[    1.480000] drm: registered panic notifier
[    1.480000] [drm] Initialized analog_drm 1.0.0 20110530 on minor 0
____________________________________________________________

and on the HDMI screen two tux image appear in the upper-left corner, furtherlly if i attach an usb mouse to the OTG port it doesn't light up. What's the problem?

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi,

    Please ask your question over at Digilent as it is referenced to their material.

    Thank you,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi,

    Please ask your question over at Digilent as it is referenced to their material.

    Thank you,

    Josh