Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Simple Adder Control Signals
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 311 views
  • Users 0 members are here
Related

Simple Adder Control Signals

Former Member
Former Member over 12 years ago

Hi all,

I am new to the Zedboard and am working up to transferring a complex hardware accelerator I currently have working on a regular FPGA board.


Anyway I want to walk before I can run so have done the speedway tutorials and am now toying around with small projects. My first of which being an simple adder accelerator:
-Send 2 numbers to the pl, to reg a and b
-the pl adds the numbers
-an interrupt signals the computation has finished.
-PS reads the result from reg c



For this design I am using 3 registers (a,b,c) in the AXI interconnect, I have created the IP templates using CIP.



Basically though what is the best way send a control signal to enable the addition to the PL. So how should I signal to the PL adder that I have loaded the two numbers in reg a and b and now want to add them?
-Should I create a 1bit signal GPIO interconnect, add a 4th 4 bit control register? or is there a more 'stylish' way to do this by using the BUS2IPdata signals?
-Or is there another way to create custom PS to PL control enable signals?

Many thanks
Sam



  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    So my current idea is:

    -Build a switch based on the BUS2IPWrCE, so when this is asserted to write to reg B I can then signal an enable signal to my adder? Or will I run into some concurrency issues with the data not being fully written straight away?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    So my current idea is:

    -Build a switch based on the BUS2IPWrCE, so when this is asserted to write to reg B I can then signal an enable signal to my adder? Or will I run into some concurrency issues with the data not being fully written straight away?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data