Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Synthesis tool not utilizing RAMB18
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 477 views
  • Users 0 members are here
Related

Synthesis tool not utilizing RAMB18

martingaraj
martingaraj over 10 years ago

I have a design with multiple buffers (128 element-long arrays storing 32 bit numbers) and during the synthesis I have came across following warning in the Synthesis Log:

ROM "read_buffer_reg[0]" won't be mapped to RAM because address size (32) is larger than maximum supported(18)
ROM "read_buffer_reg[1]" won't be mapped to RAM because address size (32) is larger than maximum supported(18)
... all the way to 127

I have somehow assumed, that the reason, why it cannot be mapped to RAM is that element size is 32 bits, so I have broken down the buffer into 2 smaller buffers,128 element-long buffers with 16 bit value per element. But the problem persists:

ROM "read_buffer_1_reg[0]" won't be mapped to RAM because address size (32) is larger than maximum supported(18)
ROM "read_buffer_1_reg[1]" won't be mapped to RAM because address size (32) is larger than maximum supported(18)
... all the way to 127


The trick seems to be in the "address size", but my buffers are long only 128 elements, that should be easily addressable by 1 byte (only 7 bits actually).

So is there a way to make the Synthesis Tool utilize the RAMB instead of other logic when it comes to such buffers?



P.S.
I have tried the following

ttype mem_buffer_short is array (0 to 127) of std_logic_vector(15 downto 0);
tsignal read_buffer_0 : mem_buffer_short;
tsignal read_buffer_1 : mem_buffer_short;
tattribute ram_style: string;
tattribute ram_style of read_buffer_0: signal is "block";
tattribute ram_style of read_buffer_1: signal is "block";


but I got the following message

WARNING: [Synth 8-3514] cannot infer block ram on a non-memory variable 'read_buffer_0' [c:/xilinx_projects_2014/fft_generator_test_01/ip_vga_axi_driver_3.6/src/VGA_stream.vhd:219]
INFO: [Synth 8-4472] Detected and applied attribute ram_style = block [c:/xilinx_projects_2014/fft_generator_test_01/ip_vga_axi_driver_3.6/src/VGA_stream.vhd:216]
WARNING: [Synth 8-3514] cannot infer block ram on a non-memory variable 'read_buffer_1' [c:/xilinx_projects_2014/fft_generator_test_01/ip_vga_axi_driver_3.6/src/VGA_stream.vhd:220]
INFO: [Synth 8-4472] Detected and applied attribute ram_style = block [c:/xilinx_projects_2014/fft_generator_test_01/ip_vga_axi_driver_3.6/src/VGA_stream.vhd:217]

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Martin,

     

    This is really a Xilinx tools specific question. I think you will find a broader and more knowledgeable audience on one of the Xilinx Community Forums targeted to the tools: 

     

    https://forums.xilinx.com/

     

    -Gary