Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design General Zedboard, and ADC and DAC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 885 views
  • Users 0 members are here
Related

General Zedboard, and ADC and DAC

e14 Contributor
e14 Contributor over 11 years ago

Hi all,

I am thinking of using Zedboard and Maxim Integrated Fresno ADC and Carmel DAC together to make a simple feedback loop in a system. I haven't bought any of them yet. I will be connecting the ADC and DAC using 2 of the PL Pmods on the Zedboard (JA1 and JB1). Do you foresee any problem with this?

I am familiar with FPGAs, but have never used a Programmable SoC. Like an FPGA, can I use an HDL with Zynq?

In the Zedboard manual, it mentions a 100MHz oscillator for PL. I can use this clock in my program, right? Hence, Zedboard does not have to be connected to the computer for clocking?

Finally, can I set the SPI clock frequency to any value I want for the ADC and DAC connected through PL Pmods?

I would appreciate any answer to any of my questions!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    i use pmod max5216(DAC)and max11205(ADC) that Produced by the company maxim that this company get me project file but in this project every pmod can not work togheter i need a project that two port pmod Setting up together untill i can use DAC and ADC Simultaneous can you help me ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    i use pmod max5216(DAC)and max11205(ADC) that Produced by the company maxim that this company get me project file but in this project every pmod can not work togheter i need a project that two port pmod Setting up together untill i can use DAC and ADC Simultaneous can you help me ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Look at the response to one of you other duplicate posts on this subject for an answer: http://zedboard.org/content/adc-and-dac-pmod

     

    Please do not post the same question to multiple threads or forums on the site.

     

    -Gary