Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Blue done LED  never
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 1162 views
  • Users 0 members are here
Related

Blue done LED  never

eddydw
eddydw over 9 years ago

Hi

I copied the original SD card image to an SD card and inserted it in the SD slot on the ZED board.

The jumpers are set to boot from SD card as follows :

MODE3 (JP10) shunted to 3.3V
MODE2 (JP9) shunted to 3.3V
All other MODE pins shunted to GND.

The uart terminal does not show a connection and the Blue led (DONE pin) never light up

Does this mean that the board is broken(Zynq does not boot)?

What cnn be the root cause? Am I missing something

Thx

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi Eddy,

    I have run into this exact problem before with improperly formatted SD cards.

    Make sure to perform a full format (usually a quick format works but sometimes it does not) of the SD card using FAT or FAT32 file systems.

    If that does not work either, you can more reliably determine if there is something wrong with the Zynq-7000 All Programmable SoC device by trying to connect to it from Vivado Hardware Manager using the built in USB-JTAG interface.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 9 years ago

    Hi Eddy,

    I have run into this exact problem before with improperly formatted SD cards.

    Make sure to perform a full format (usually a quick format works but sometimes it does not) of the SD card using FAT or FAT32 file systems.

    If that does not work either, you can more reliably determine if there is something wrong with the Zynq-7000 All Programmable SoC device by trying to connect to it from Vivado Hardware Manager using the built in USB-JTAG interface.

    Regards,

    -Kevin