Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design UART0 routed to PL via EMIO does not send any data out
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 2653 views
  • Users 0 members are here
Related

UART0 routed to PL via EMIO does not send any data out

fayyazrafiq
fayyazrafiq over 12 years ago

Hi,

I am having the EMIO problem. I wanted to use PS UART0 via EMIO and connected it to PL side package pins in XPS, but i could see any data out after several tries.  I am using XPS 14.5 and SDK 14.5 with ZEDBOARD.

I also tried the XMD debugger and I can see the UART0 data out via PL package pins. I don't know where is the problem but i am struggling this problem from one week. please help me.

Any help is highly appreciated.

Regards
Fayyaz

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Fayyaz,

     

    I do not have 14.5 loaded but I do have 14.7, so I built up a new design using PlanAhead, in a similar fashion to the Concepts, Tools and Techniques tutorial for 14.5 located here: http://www.zedboard.org/design/1521/11

     

    In addition to the base design from the tutorial I added UART 0 with EMIO connections. I made the UART0 TX and RX ports 'External' and exited XPS. I then created a Top HDL file and used the signal names assigned there to add constraints to connect the UART 0 TX and RX signals to one of the ZedBoard PMOD connectors in a constraints file I created. I implemented the design and generated a bitstream and then 'exported' the design to SDK. There I generated a basic 'Hello World' application. Note that when you enable UART0 it will become the sdin/sdout port for the SDK applications. I connected a terminal to an RS232 converter connected to the Zedboard PMOD with the UART0 TX and RX signals, loaded the FPGA bitstream, and then ran the 'Hello World' application. I get the "Hello World" output on the terminal connected to UART0 via the RS232 converter on the PMOD connection.

     

    I have done a similar design with Vivado 2031.4 and it works as well.

     

    You might want to complete a like design to verify your tools and hardware operation. Please make sure you have made the UART0 ports External, added a constraints file, loaded the FPGA bitstream, and remember that the PMOD signals are LVCMOS33 signal levels. If you are still having issues one thing I have seen cause odd issues is a corrupt Xilinx tools installation. If you still have the archive file you downloaded to install your Xilinx tools you might want to verify that the MD5 sum is correct and matches the one published on the Xilinx download site.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello Fayyaz,

     

    I do not have 14.5 loaded but I do have 14.7, so I built up a new design using PlanAhead, in a similar fashion to the Concepts, Tools and Techniques tutorial for 14.5 located here: http://www.zedboard.org/design/1521/11

     

    In addition to the base design from the tutorial I added UART 0 with EMIO connections. I made the UART0 TX and RX ports 'External' and exited XPS. I then created a Top HDL file and used the signal names assigned there to add constraints to connect the UART 0 TX and RX signals to one of the ZedBoard PMOD connectors in a constraints file I created. I implemented the design and generated a bitstream and then 'exported' the design to SDK. There I generated a basic 'Hello World' application. Note that when you enable UART0 it will become the sdin/sdout port for the SDK applications. I connected a terminal to an RS232 converter connected to the Zedboard PMOD with the UART0 TX and RX signals, loaded the FPGA bitstream, and then ran the 'Hello World' application. I get the "Hello World" output on the terminal connected to UART0 via the RS232 converter on the PMOD connection.

     

    I have done a similar design with Vivado 2031.4 and it works as well.

     

    You might want to complete a like design to verify your tools and hardware operation. Please make sure you have made the UART0 ports External, added a constraints file, loaded the FPGA bitstream, and remember that the PMOD signals are LVCMOS33 signal levels. If you are still having issues one thing I have seen cause odd issues is a corrupt Xilinx tools installation. If you still have the archive file you downloaded to install your Xilinx tools you might want to verify that the MD5 sum is correct and matches the one published on the Xilinx download site.

     

    -Gary