Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zynq Boot Image
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 360 subscribers
  • Views 969 views
  • Users 0 members are here
Related

Zynq Boot Image

e14 Contributor
e14 Contributor over 9 years ago

Hi,

I have a model in Simulink that I can run in Zedboard. I have configurated the Ethernet subnet in Zedboard too. But when I create a new Zynq Boot Image and try to execute the interfaz model on the Zedboard, I have a problem with the network because the system not connect and I recive the following message:

Error occurred while executing External Mode MEX-file 'ext_comm': Failed to connect to the target. Possible reasons for the failure: a) The target is not switched on. b) The target is not connected to your host machine. c) The application for the model is not running on the target. You might have clicked the Stop button. Caused by: An error occurred attempting to open an rtIOStream. More detail may be reported in the MATLAB command window

I think my problem is in the boot configuration but I don't know how to solve it. Can you help me?

Thanks and regards,

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 9 years ago

    If I understand your question, you want to modify the Zynq boot image used with the  MathWorks Zynq Support Packages and External Mode.

    To my knowledge there is not support for this.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 9 years ago

    If I understand your question, you want to modify the Zynq boot image used with the  MathWorks Zynq Support Packages and External Mode.

    To my knowledge there is not support for this.

    /Matt