Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design FIR Compiler 7.1 in Vivado 2013.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 1207 views
  • Users 0 members are here
Related

FIR Compiler 7.1 in Vivado 2013.2

e14 Contributor
e14 Contributor over 13 years ago

Hi

I was wondering if anyone has managed to use the FIR Compiler IP in Vivado 2013.2. The overall aim of my project is to perform audio filtering of data connected from the audio codec. At the moment though, I am just focusing on trying to get anything to come out of the other side of the filter!

I have found no examples online of how to use it, and do not find the information in the product guide very helpful!

My understanding is that to send data from the PS to the filter, and then get it back again, you would place the following blocks:
http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fir_connection.png

First off - is this correct?!

Deleting the FIR block and just connecting the AXI_STR_TXD and AXI_STR_RXD ports on the AXI_Stream FIFO together, I am able to send and then receive data. When I stick the FIR in though, nothing comes out of it. If it is connected correctly, then presumably something is wrong in the settings of the IP block.

Has anyone done anything like this before who would like to share ...?!

Thanks

Kenny

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, I've a problem too with fir compiler. The line s_axis_data_tready (which in an output moved by the filter itself) does not move. so I see Input, but no output from the filter. I've opened a discussion on Xilinx forum...hope they answer soon. http://forums.xilinx.com/t5/7-Series-FPGAs/FIR-COMPILER-7-1-problem-on-VIVADO-2013-2/td-p/345843

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, I've a problem too with fir compiler. The line s_axis_data_tready (which in an output moved by the filter itself) does not move. so I see Input, but no output from the filter. I've opened a discussion on Xilinx forum...hope they answer soon. http://forums.xilinx.com/t5/7-Series-FPGAs/FIR-COMPILER-7-1-problem-on-VIVADO-2013-2/td-p/345843