Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design FIR Compiler 7.1 in Vivado 2013.2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 1195 views
  • Users 0 members are here
Related

FIR Compiler 7.1 in Vivado 2013.2

e14 Contributor
e14 Contributor over 12 years ago

Hi

I was wondering if anyone has managed to use the FIR Compiler IP in Vivado 2013.2. The overall aim of my project is to perform audio filtering of data connected from the audio codec. At the moment though, I am just focusing on trying to get anything to come out of the other side of the filter!

I have found no examples online of how to use it, and do not find the information in the product guide very helpful!

My understanding is that to send data from the PS to the filter, and then get it back again, you would place the following blocks:
http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fir_connection.png

First off - is this correct?!

Deleting the FIR block and just connecting the AXI_STR_TXD and AXI_STR_RXD ports on the AXI_Stream FIFO together, I am able to send and then receive data. When I stick the FIR in though, nothing comes out of it. If it is connected correctly, then presumably something is wrong in the settings of the IP block.

Has anyone done anything like this before who would like to share ...?!

Thanks

Kenny

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, I've a problem too with fir compiler. The line s_axis_data_tready (which in an output moved by the filter itself) does not move. so I see Input, but no output from the filter. I've opened a discussion on Xilinx forum...hope they answer soon. http://forums.xilinx.com/t5/7-Series-FPGAs/FIR-COMPILER-7-1-problem-on-VIVADO-2013-2/td-p/345843

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi

    I have still not got anywhere! I have tested a very similar system in System Generator

    http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fir_fifo_sysgen.png

    When I apply an impulse to the system, it works as it should

    http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fir_fifo_sysgen_wavescope1.png

    and

    http://personal.strath.ac.uk/kenneth.barlee/zed_posts/fir_fifo_sysgen_wavescope2.png


    ....so I really have no idea why the same thing is not working in Vivado! I have contacted Xilinx too - if I get a reply I will post it

    Kenny

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Did you guys managed to find any solution for this problem? I am struggling with the same thing at the moment. Cannot find good guides for the issue in the web. I hope you could share your solution to the problem, if you've got one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Have any one got a working model of FIR filter??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi..
    finally i have completed a model for fir filtering uaing the fir compiler. Instead of using the fifo i have used dma. the model works fine.

    The following is the link to the solution
    http://forums.xilinx.com/t5/Embedded-Processor-System-Design/FIR-compiler-and-PS/m-p/547409#M13571

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    http://forums.xilinx.com/t5/Embedded-Processor-System-Design/FIR-compiler-and-PS/td-p/544565

    Solution to the above problem can be found in this xilinx page.