Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Configure PL Clocks When Using Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 594 views
  • Users 0 members are here
Related

Configure PL Clocks When Using Linux

Former Member
Former Member over 13 years ago

Hello,

How do I configure FCLK0 when using the Zedboard with Linux?

I have designed and tested on bare metal a peripheral I have created. For its use I have configured FCLK0 to be 10MHz. The clock configuration works and has been verified on the oscilloscope. 

I have created an FSBL from the same hardware, and used that to create a boot.bin. I've replaced the default boot.bin with my new one on the SD card.

While the system boots I see the blue light go on, then on the oscope I can see the FCLK0 (I have it routed to a pin on a pMod) stabilize at 10MHz. Seems great, but a few seconds later the clock reconfigures to 100MHz (stock).

Any insight to why this is happening, and what I can do to fix it would be greatly appreciated.

Sincereley, Phil

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    When you say, "I have configured FCLK0 to be 10MHz," how are you doing that? There are ways to do this in software, but you really should go back to the hardware platform in XPS, change it there, and then regenerate the hardware platform and BSP.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to bhfletcher

    Thank you for expressing interest in helping me. I've got my system working with a bit of a hack- instead of reconfiguring FCLK0, I leave it at 100MHz and added in a 'clock wizard' to the system to bump it down to 10Mhz- my project is working now. I'd still like to know if you have any ideas off the top of your head, so I will explain in more detail what I am experiencing.

    I configured it in the hardware, regenerated hardware platform and BSP. At that  point the 10MHz is correctly and verifiably set when using the bare metal. When use that hardware to generate an FSBL and make a boot.bin out of the new FSBL, bitfile, and a copy of u-boot the system configures for 10MHz (seen on scope) but it only sticks for about 10 seconds, at which point some part of the system sets it back to 100MHz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago in reply to bhfletcher

    Thank you for expressing interest in helping me. I've got my system working with a bit of a hack- instead of reconfiguring FCLK0, I leave it at 100MHz and added in a 'clock wizard' to the system to bump it down to 10Mhz- my project is working now. I'd still like to know if you have any ideas off the top of your head, so I will explain in more detail what I am experiencing.

    I configured it in the hardware, regenerated hardware platform and BSP. At that  point the 10MHz is correctly and verifiably set when using the bare metal. When use that hardware to generate an FSBL and make a boot.bin out of the new FSBL, bitfile, and a copy of u-boot the system configures for 10MHz (seen on scope) but it only sticks for about 10 seconds, at which point some part of the system sets it back to 100MHz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bhfletcher
    0 bhfletcher over 13 years ago in reply to Former Member

    Sounds like the FSBL is hard-coded for 100 MHz. What version of Xilinx tools are you using?

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to bhfletcher

    I'm using 14.4. I just find it strange that I see the 10MHz momentarily. Thanks for the suggestions, my system is working now so I guess I'll just go with that and enjoy that it is no longer broken.
    -Phil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer