Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Changing FCLK issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1180 views
  • Users 0 members are here
Related

Changing FCLK issue

Former Member
Former Member over 13 years ago

Hello,

I am trying to change the FCLK_CLK0 clock from 100 MHz to 200/250 MHz. This clock is connected to an AXI Interconnect, AXI CDMA and a template-generated peripheral (Default AXI Memory mapped). The issue is that my program works at 100 MHZ (I can create a DMA transfer from peripheral to DDR Mem) but at 200/250Mhz, the CDMA reports transfer error.
The issue seems to be that somehow, EDK is not imposing a timing constraint on my peripheral to work at that frequency. I am saying this because in PlanAhead Project Summary, in the Implemented Timing section it says "All constraints were met. Maximum Frequency: 100.291 Mhz", which is odd.
Investigating further, I have noticed there is a file, ./cryptozed.srcs/sources_1/edk/system/implementation/system_processing_system7_0_wrapper.ncf, which has the following lines:
############################################################################
# Clock constraints                                                        #
############################################################################
NET FCLK_CLK0 TNM_NET = clk_fpga_0;
TIMESPEC TS_clk_fpga_0 = PERIOD clk_fpga_0 100000 kHz;

I'm using PlanAhead 14.4.1

Any ideas?

I really appreciate any help you can provide,
Nicolae Rosia.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    Given that this is a Xilinx tool issue, I suggest you also open a Xilinx WebCase in parallel with this forum posting.

    www.xilinx.com/webcase

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    Given that this is a Xilinx tool issue, I suggest you also open a Xilinx WebCase in parallel with this forum posting.

    www.xilinx.com/webcase

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data