Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Changing FCLK issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 359 subscribers
  • Views 1179 views
  • Users 0 members are here
Related

Changing FCLK issue

Former Member
Former Member over 13 years ago

Hello,

I am trying to change the FCLK_CLK0 clock from 100 MHz to 200/250 MHz. This clock is connected to an AXI Interconnect, AXI CDMA and a template-generated peripheral (Default AXI Memory mapped). The issue is that my program works at 100 MHZ (I can create a DMA transfer from peripheral to DDR Mem) but at 200/250Mhz, the CDMA reports transfer error.
The issue seems to be that somehow, EDK is not imposing a timing constraint on my peripheral to work at that frequency. I am saying this because in PlanAhead Project Summary, in the Implemented Timing section it says "All constraints were met. Maximum Frequency: 100.291 Mhz", which is odd.
Investigating further, I have noticed there is a file, ./cryptozed.srcs/sources_1/edk/system/implementation/system_processing_system7_0_wrapper.ncf, which has the following lines:
############################################################################
# Clock constraints                                                        #
############################################################################
NET FCLK_CLK0 TNM_NET = clk_fpga_0;
TIMESPEC TS_clk_fpga_0 = PERIOD clk_fpga_0 100000 kHz;

I'm using PlanAhead 14.4.1

Any ideas?

I really appreciate any help you can provide,
Nicolae Rosia.

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    Reading through this again, I want to clarify.  I think the best and easiest way to change FCLK_CLK0 is to go all the way back to the Hardware platform and set it there.  You can modify the registers and do this in software, but then you may run into the problem where the entire system is not knowledgeable of the new clock setting.

     

    In PlanAhead, edit your embedded system.  In the Zynq tab, click on the Clock Generation block.  Expand the PL Fabric Clocks.  Change FCLK_CLK0 to your desired frequency.  Take note to see if the "Actual" matches your "Requested."  Next, click Validate Clocks.  Then click OK, then close XPS.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    Reading through this again, I want to clarify.  I think the best and easiest way to change FCLK_CLK0 is to go all the way back to the Hardware platform and set it there.  You can modify the registers and do this in software, but then you may run into the problem where the entire system is not knowledgeable of the new clock setting.

     

    In PlanAhead, edit your embedded system.  In the Zynq tab, click on the Clock Generation block.  Expand the PL Fabric Clocks.  Change FCLK_CLK0 to your desired frequency.  Take note to see if the "Actual" matches your "Requested."  Next, click Validate Clocks.  Then click OK, then close XPS.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data