Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Run Program without Simulink
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 597 views
  • Users 0 members are here
Related

Run Program without Simulink

e14 Contributor
e14 Contributor over 10 years ago

Hi all,

does anybody know if it's possible to store a simulink model, i.e. the generated c-code and bitstream (for the fpga), on the zedboard? I want the zedboard to boot and execute a model in external mode without simulink.

Regards, w3rt3

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for your answer DSP_1!

    My algorithm and Simulink model work fine in external model, i even can disconnect Matlab from the ZedBoard and the programm is still running perfectly. To build this standalone application i used:

    setenv('XILINX_ARM_CROSS_COMPILE','C:\Xilinx\SDK\2014.4\gnu\arm\nt\bin');
    zynq('Linux','128.130.200.181','root','root','/home/root');

    The problem is the following. When I restart the ZedBoard, my application is gone and I have to program the board with simulink again. I want the application to run automatically after the ZedBoard finished booting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for your answer DSP_1!

    My algorithm and Simulink model work fine in external model, i even can disconnect Matlab from the ZedBoard and the programm is still running perfectly. To build this standalone application i used:

    setenv('XILINX_ARM_CROSS_COMPILE','C:\Xilinx\SDK\2014.4\gnu\arm\nt\bin');
    zynq('Linux','128.130.200.181','root','root','/home/root');

    The problem is the following. When I restart the ZedBoard, my application is gone and I have to program the board with simulink again. I want the application to run automatically after the ZedBoard finished booting.