Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Run Program without Simulink
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 598 views
  • Users 0 members are here
Related

Run Program without Simulink

e14 Contributor
e14 Contributor over 10 years ago

Hi all,

does anybody know if it's possible to store a simulink model, i.e. the generated c-code and bitstream (for the fpga), on the zedboard? I want the zedboard to boot and execute a model in external mode without simulink.

Regards, w3rt3

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago
    External mode is meant to connect Simulink to Zynq PS over Ethernet in order to tune parameters, and monitor the algorithm running in PL through an AXI interface. If your algorithm is already fully operational and needs no further debugging, then you simply run the executable on Linux on the ARM processor. The generated embedded software includes AXI driver code, generated from the AXI driver blocks, that controls the HDL IP core.
     
    This example is a good introduction to the MathWorks hardware-software codesign workflow:
     
    http://www.mathworks.com/help/hdlcoder/examples/getting-started-with-hardware-software-codesign-workflow-for-xilinx-zynq-platform.html?s_tid=srchtitle
     
    Contact fpga_expert@mathworks.com for more details.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for your answer DSP_1!

    My algorithm and Simulink model work fine in external model, i even can disconnect Matlab from the ZedBoard and the programm is still running perfectly. To build this standalone application i used:

    setenv('XILINX_ARM_CROSS_COMPILE','C:\Xilinx\SDK\2014.4\gnu\arm\nt\bin');
    zynq('Linux','128.130.200.181','root','root','/home/root');

    The problem is the following. When I restart the ZedBoard, my application is gone and I have to program the board with simulink again. I want the application to run automatically after the ZedBoard finished booting.