Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Adding a 640x480 camera to your Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 357 subscribers
  • Views 3134 views
  • Users 0 members are here
Related

Adding a 640x480 camera to your Zedboard

Former Member
Former Member over 13 years ago

Hi all.

I've adapted a low-cost VGA camera module to interface with the Zedboard over PMODA and PMODB. About $15 worth of hardware and no soldering to give your Zedboard eyes!

As the PL has four PMODs you should even be able to give it stereo vision.

It is currently showing a picture on the Zedboards Analogue VGA out, but I want to test and polish it just a little more before I release the code - tweak some of the camera's registers values and so on.

I've added a community project, and will put the code up as soon it is ready. If in the short term you would like the code, just email or message me.

Kind regards

Mike

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    The project is pretty much complete - I would like to add a way to store the image in the DDR memory, but that is beyond my skills at the moment.

    I've also discovered that the cameras I am using do not have infra-red filters, so the colours are all mixed up.

    Also, although the cameras are 640x480 on a 25MHz clock they are only 30 frames per second, as a pixel requires two clocks to transfer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    The project is pretty much complete - I would like to add a way to store the image in the DDR memory, but that is beyond my skills at the moment.

    I've also discovered that the cameras I am using do not have infra-red filters, so the colours are all mixed up.

    Also, although the cameras are 640x480 on a 25MHz clock they are only 30 frames per second, as a pixel requires two clocks to transfer.