Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Run-Time Reconfiguration on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 423 views
  • Users 0 members are here
Related

Run-Time Reconfiguration on ZedBoard

e14 Contributor
e14 Contributor over 10 years ago

Hi everybody,
I'm working with a ZedBoard and my goal is to set up a run-time reconfigurable platform. I need a processor with some reconfigurable accelerator on its side.
I'm new to this platform and Xilinx tools, so I'm asking your help about important points:

-it's easier to use the included ARM dual-core processor or to use a MicroBlaze soft-processor to set-up a reconfigurable architecture?

-I found lots of guides and documentation by Xilinx and ZedBoard, but what is the workflow you suggest me to start working on this new platform?

-do you know any step by step tutorial to start working using the tipical Xilinx workflow on a ZedBoard?

Thanks in advanace!

  • Sign in to reply
  • Cancel
  • narrucmot
    0 narrucmot over 10 years ago

    Hi Emilio,

    The best place to start is probably with Xilinx UG947(http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug947-vivado-partial-reconfiguration-tutorial.pdf).  Xilinx UG909 (http://www.xilinx.com/support/documentation/sw_manuals/xilinx2015_4/ug909-vivado-partial-reconfiguration.pdf) will also be good for reference and XAPP1159 (http://www.xilinx.com/support/documentation/application_notes/xapp1159-partial-reconfig-hw-accelerator-zynq-7000.pdf) or XAPP1231 (http://www.xilinx.com/support/documentation/application_notes/xapp1231-partial-reconfig-hw-accelerator-vivado.pdf) describe using partial reconfiguration in Zynq and with Linux for a video-based design.  This webpage (http://www.xilinx.com/products/design-tools/vivado/implementation/partial-reconfiguration.html) is also a good portal for all things related to partial reconfiguration in Xilinx devices.

    I hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to narrucmot

    Thanks for you answer!
    I agree with your suggestion, I'm studying the documents you linked and I'll try to follow step by step the tutorial, trying to understand each command.
    I'm still confused about two things:

    -if use the embedded ARM cores or not (using the programmable logic only)

    -how to use the SDK to develop applications capable to take advantage of the reconfigurable modules

    Thanks again, every other suggestion will be welcome.
    Emilio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I followed a tutorial to create an HW accelerator for the PL in order to work together with the ARM PS.
    I used the following work-flow:

    ->VIVADO HLS:
    -->c simulation
    -->c synthesis
    -->c/rtl co-simulation
    -->export ip

    ->VIVADO DESIGN SUITE
    -->create block design
    -->generate output file
    -->generate hdl wrapper
    -->generate bitstream
    -->export hardware
    -->launch sdk

    ->XILINX SDK
    -->create bsp
    -->create application

    Now I have some questions:

    - If I want to use the PCAP interface to partially reconfigure the PL run-time how have I to modify the work-flow?

    - Have I to add some specific block in the block design to be able to use the PCAP?

    Thanks in advance