Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design gpio offset
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 1207 views
  • Users 0 members are here
Related

gpio offset

Former Member
Former Member over 12 years ago

Hello,
How do you determine the offset of the gpioxx.
#!/bin/bash
#This appears to work with fpga.bin loaded
echo "++ Exporting switches "
for i in 0 1 2 3 4 5 6 7;
do
        sw=$(($i+65));
        echo $sw > /sys/class/gpio/export;
done;

#!/bin/sh
value=0;
for i in 0 1 2 3 4 5 6 7;
do
        sw=$((72-$i));
        sw_tmp=`cat /sys/class/gpio/gpio$sw/value`;
        value=$(($value*2));
        value=$(($value+$sw_tmp));
done;
printf "0x%x %d
" $value $value;
This work with the system.ucf.
NET processing_system7_0_GPIO_pin[11]tLOC = F22  | IOSTANDARD="LVCMOS25";  # "SW0"
NET processing_system7_0_GPIO_pin[12]tLOC = G22  | IOSTANDARD="LVCMOS25";  # "SW1"
NET processing_system7_0_GPIO_pin[13]tLOC = H22  | IOSTANDARD="LVCMOS25";  # "SW2"
NET processing_system7_0_GPIO_pin[14]tLOC = F21  | IOSTANDARD="LVCMOS25";  # "SW3"
NET processing_system7_0_GPIO_pin[15]tLOC = H19  | IOSTANDARD="LVCMOS25";  # "SW4"
NET processing_system7_0_GPIO_pin[16]tLOC = H18  | IOSTANDARD="LVCMOS25";  # "SW5"
NET processing_system7_0_GPIO_pin[17]tLOC = H17  | IOSTANDARD="LVCMOS25";  # "SW6"
NET processing_system7_0_GPIO_pin[18]tLOC = M15  | IOSTANDARD="LVCMOS25";  # "SW7"

NET processing_system7_0_GPIO_pin[19]tLOC = T22  | IOSTANDARD="LVCMOS33";  # "LD0"
NET processing_system7_0_GPIO_pin[20]tLOC = T21  | IOSTANDARD="LVCMOS33";  # "LD1"
NET processing_system7_0_GPIO_pin[21]tLOC = U22  | IOSTANDARD="LVCMOS33";  # "LD2"
NET processing_system7_0_GPIO_pin[22]tLOC = U21  | IOSTANDARD="LVCMOS33";  # "LD3"
NET processing_system7_0_GPIO_pin[23]tLOC = V22  | IOSTANDARD="LVCMOS33";  # "LD4"
NET processing_system7_0_GPIO_pin[24]tLOC = W22  | IOSTANDARD="LVCMOS33";  # "LD5"
NET processing_system7_0_GPIO_pin[25]tLOC = U19  | IOSTANDARD="LVCMOS33";  # "LD6"
NET processing_system7_0_GPIO_pin[26]tLOC = U14  | IOSTANDARD="LVCMOS33";  # "LD7"
I can not get the LED to work.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Take a look at the Zynq Linux Speedway, Lab 3.1 and see if that is helpful. It is based on an older version of the tools/linux but may still be on target.The Implementing Linux on the Zynq 7000 SoC can be downloaded from here:

     

    http://www.zedboard.org/support/trainings-and-videos

     

    Let us know how it works.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Take a look at the Zynq Linux Speedway, Lab 3.1 and see if that is helpful. It is based on an older version of the tools/linux but may still be on target.The Implementing Linux on the Zynq 7000 SoC can be downloaded from here:

     

    http://www.zedboard.org/support/trainings-and-videos

     

    Let us know how it works.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data