Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design gpio offset
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 1207 views
  • Users 0 members are here
Related

gpio offset

Former Member
Former Member over 12 years ago

Hello,
How do you determine the offset of the gpioxx.
#!/bin/bash
#This appears to work with fpga.bin loaded
echo "++ Exporting switches "
for i in 0 1 2 3 4 5 6 7;
do
        sw=$(($i+65));
        echo $sw > /sys/class/gpio/export;
done;

#!/bin/sh
value=0;
for i in 0 1 2 3 4 5 6 7;
do
        sw=$((72-$i));
        sw_tmp=`cat /sys/class/gpio/gpio$sw/value`;
        value=$(($value*2));
        value=$(($value+$sw_tmp));
done;
printf "0x%x %d
" $value $value;
This work with the system.ucf.
NET processing_system7_0_GPIO_pin[11]tLOC = F22  | IOSTANDARD="LVCMOS25";  # "SW0"
NET processing_system7_0_GPIO_pin[12]tLOC = G22  | IOSTANDARD="LVCMOS25";  # "SW1"
NET processing_system7_0_GPIO_pin[13]tLOC = H22  | IOSTANDARD="LVCMOS25";  # "SW2"
NET processing_system7_0_GPIO_pin[14]tLOC = F21  | IOSTANDARD="LVCMOS25";  # "SW3"
NET processing_system7_0_GPIO_pin[15]tLOC = H19  | IOSTANDARD="LVCMOS25";  # "SW4"
NET processing_system7_0_GPIO_pin[16]tLOC = H18  | IOSTANDARD="LVCMOS25";  # "SW5"
NET processing_system7_0_GPIO_pin[17]tLOC = H17  | IOSTANDARD="LVCMOS25";  # "SW6"
NET processing_system7_0_GPIO_pin[18]tLOC = M15  | IOSTANDARD="LVCMOS25";  # "SW7"

NET processing_system7_0_GPIO_pin[19]tLOC = T22  | IOSTANDARD="LVCMOS33";  # "LD0"
NET processing_system7_0_GPIO_pin[20]tLOC = T21  | IOSTANDARD="LVCMOS33";  # "LD1"
NET processing_system7_0_GPIO_pin[21]tLOC = U22  | IOSTANDARD="LVCMOS33";  # "LD2"
NET processing_system7_0_GPIO_pin[22]tLOC = U21  | IOSTANDARD="LVCMOS33";  # "LD3"
NET processing_system7_0_GPIO_pin[23]tLOC = V22  | IOSTANDARD="LVCMOS33";  # "LD4"
NET processing_system7_0_GPIO_pin[24]tLOC = W22  | IOSTANDARD="LVCMOS33";  # "LD5"
NET processing_system7_0_GPIO_pin[25]tLOC = U19  | IOSTANDARD="LVCMOS33";  # "LD6"
NET processing_system7_0_GPIO_pin[26]tLOC = U14  | IOSTANDARD="LVCMOS33";  # "LD7"
I can not get the LED to work.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hello All
    My problem is that I cannot get the 8 leds to work.  The 8 switches are working.
    ls /sys/class/gpio/
    export    gpiochip0  unexport
    root@zedboard:/etc/init.d# export_sw
    ++ Exporting switches
    root@zedboard:/etc/init.d# cat /usr/bin/export_sw
    #!/bin/bash
    #This appears to work with fpga.bin loaded
    echo "++ Exporting switches "
    for i in 0 1 2 3 4 5 6 7;
    do
            sw=$(($i+65));
            echo $sw > /sys/class/gpio/export;
    done;
    root@zedboard:/etc/init.d# ls /sys/class/gpio/
    export    gpio66    gpio68    gpio70    gpio72       unexport
    gpio65    gpio67    gpio69    gpio71    gpiochip0
    cat /usr/bin/read_sw
    #!/bin/sh
    value=0;
    for i in 0 1 2 3 4 5 6 7;
    do
            sw=$((72-$i));
            sw_tmp=`cat /sys/class/gpio/gpio$sw/value`;
            value=$(($value*2));
            value=$(($value+$sw_tmp));
    done;
    printf "0x%x %d
    " $value $value;
    setting the switches 10101010
    root@zedboard:/etc/init.d# read_sw
    0xaa 170

    I recently built a system.bit and with meta-topic a fpga.bin
    It appears that the fpga.bin is being loaded since I have a script
    ck_fpga  that I extracted from /etc/init.d/fpga-image-load.sh
    #!/bin/sh
    #extracted from /etc/init.d/fpga-image-load.sh
    #used to check if fpga.bin was loaded.
    result=`cat     /sys/devices/amba.[0123]/f8007000.devcfg/prog_done`
    echo $result
    root@zedboard:~# ./ck_fpga
    1

    I would think that 8 Leds would be 73-80.
    cat /usr/bin/export_led
    #!/bin/bash
    #This appears to work with fpga.bin loaded
    echo "++ Exporting switches "
    for i in 0 1 2 3 4 5 6 7 ;
    do
            led=$(($i+73));
            echo $led > /sys/class/gpio/export;
            echo out > /sys/class/gpio/gpio$led/direction;
    done;
    This gets errors.
    Could this be the problem ZedBoard_Linux_Design net processing_system7_0_GPIO<7>  LOC = T22 while the
    cf_adv7511_zed uses NET processing_system7_0_GPIO_pin[11].  I have gone over this many times but can not determine the offsets needed to get the 8 Leds to work.   Any and all help is appreciated. Thanks
                                               ZedBoard_Linux_Design
    system.ucf
    ############################
    #                          #
    # On-board LED's           #
    #                          #
    ############################
    net processing_system7_0_GPIO<7>  LOC = T22 | IOSTANDARD = LVCMOS33;    # LD0
    net processing_system7_0_GPIO<8>  LOC = T21 | IOSTANDARD = LVCMOS33;    # LD1
    net processing_system7_0_GPIO<9>  LOC = U22 | IOSTANDARD = LVCMOS33;    # LD2
    net processing_system7_0_GPIO<10> LOC = U21 | IOSTANDARD = LVCMOS33;    # LD3
    net processing_system7_0_GPIO<11> LOC = V22 | IOSTANDARD = LVCMOS33;    # LD4
    net processing_system7_0_GPIO<12> LOC = W22 | IOSTANDARD = LVCMOS33;    # LD5
    net processing_system7_0_GPIO<13> LOC = U19 | IOSTANDARD = LVCMOS33;    # LD6
    net processing_system7_0_GPIO<14> LOC = U14 | IOSTANDARD = LVCMOS33;    # LD7

    ############################
    #                          #
    # On-board Slide Switches  #
    #                          #
    ############################
    net processing_system7_0_GPIO<15> LOC = F22 | IOSTANDARD = LVCMOS33;    # SW0
    net processing_system7_0_GPIO<16> LOC = G22 | IOSTANDARD = LVCMOS33;    # SW1
    net processing_system7_0_GPIO<17> LOC = H22 | IOSTANDARD = LVCMOS33;    # SW2
    net processing_system7_0_GPIO<18> LOC = F21 | IOSTANDARD = LVCMOS33;    # SW3
    net processing_system7_0_GPIO<19> LOC = H19 | IOSTANDARD = LVCMOS33;    # SW4
    net processing_system7_0_GPIO<20> LOC = H18 | IOSTANDARD = LVCMOS33;    # SW5
    net processing_system7_0_GPIO<21> LOC = H17 | IOSTANDARD = LVCMOS33;    # SW6
    net processing_system7_0_GPIO<22> LOC = M15 | IOSTANDARD = LVCMOS33;    # SW7
    GPIO
        MIO GPIO MIO
            EMIO GPIO (Width) 60
    MIO 0   GPIO gpio[0] disabled
    MIO 9   GPIO gpio[9] disabled
    MIO 10   GPIO gpio[10] disabled
               .
               .
               .
    MIO 15   GPIO gpio[15] disabled
    Ports
                  Connected Port
    (IO_IF)GPIO_0 Connected to External Ports
                  External Posts::processing_system7_0_MIO
           GPIO   External Posts::processing_system7_0_GPIO IO [59:0]
           GPIO_I                                             I [59:0]
           GPIO_O                                             O [59:0]
           GPIO_T                                             O [59:0]


                                               cf_adv7511_zed
    system.ucf
    NET processing_system7_0_GPIO_pin[11]    LOC = F22  | IOSTANDARD="LVCMOS25";  # "SW0"
    NET processing_system7_0_GPIO_pin[12]    LOC = G22  | IOSTANDARD="LVCMOS25";  # "SW1"
    NET processing_system7_0_GPIO_pin[13]    LOC = H22  | IOSTANDARD="LVCMOS25";  # "SW2"
    NET processing_system7_0_GPIO_pin[14]    LOC = F21  | IOSTANDARD="LVCMOS25";  # "SW3"
    NET processing_system7_0_GPIO_pin[15]    LOC = H19  | IOSTANDARD="LVCMOS25";  # "SW4"
    NET processing_system7_0_GPIO_pin[16]    LOC = H18  | IOSTANDARD="LVCMOS25";  # "SW5"
    NET processing_system7_0_GPIO_pin[17]    LOC = H17  | IOSTANDARD="LVCMOS25";  # "SW6"
    NET processing_system7_0_GPIO_pin[18]    LOC = M15  | IOSTANDARD="LVCMOS25";  # "SW7"

    NET processing_system7_0_GPIO_pin[19]    LOC = T22  | IOSTANDARD="LVCMOS33";  # "LD0"
    NET processing_system7_0_GPIO_pin[20]    LOC = T21  | IOSTANDARD="LVCMOS33";  # "LD1"
    NET processing_system7_0_GPIO_pin[21]    LOC = U22  | IOSTANDARD="LVCMOS33";  # "LD2"
    NET processing_system7_0_GPIO_pin[22]    LOC = U21  | IOSTANDARD="LVCMOS33";  # "LD3"
    NET processing_system7_0_GPIO_pin[23]    LOC = V22  | IOSTANDARD="LVCMOS33";  # "LD4"
    NET processing_system7_0_GPIO_pin[24]    LOC = W22  | IOSTANDARD="LVCMOS33";  # "LD5"
    NET processing_system7_0_GPIO_pin[25]    LOC = U19  | IOSTANDARD="LVCMOS33";  # "LD6"
    NET processing_system7_0_GPIO_pin[26]    LOC = U14  | IOSTANDARD="LVCMOS33";  # "LD7"
    GPIO
        MIO GPIO MIO
            EMIO GPIO (Width) 32
    MIO 0   GPIO gpio[0] disabled
    MIO 9   GPIO gpio[9] disabled
    MIO 10   GPIO gpio[10] disabled
               .
               .
               .
    MIO 15   GPIO gpio[15] disabled
    Ports
                  Connected Port
    (IO_IF)GPIO_0 Connected to External Ports
           GPIO   External Posts::processing_system7_0_GPIO_pin IO [31:0]
           GPIO_I                                             I [31:0]
           GPIO_O                                             O [31:0]
           GPIO_T                                             O [31:0]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    Hello All
    My problem is that I cannot get the 8 leds to work.  The 8 switches are working.
    ls /sys/class/gpio/
    export    gpiochip0  unexport
    root@zedboard:/etc/init.d# export_sw
    ++ Exporting switches
    root@zedboard:/etc/init.d# cat /usr/bin/export_sw
    #!/bin/bash
    #This appears to work with fpga.bin loaded
    echo "++ Exporting switches "
    for i in 0 1 2 3 4 5 6 7;
    do
            sw=$(($i+65));
            echo $sw > /sys/class/gpio/export;
    done;
    root@zedboard:/etc/init.d# ls /sys/class/gpio/
    export    gpio66    gpio68    gpio70    gpio72       unexport
    gpio65    gpio67    gpio69    gpio71    gpiochip0
    cat /usr/bin/read_sw
    #!/bin/sh
    value=0;
    for i in 0 1 2 3 4 5 6 7;
    do
            sw=$((72-$i));
            sw_tmp=`cat /sys/class/gpio/gpio$sw/value`;
            value=$(($value*2));
            value=$(($value+$sw_tmp));
    done;
    printf "0x%x %d
    " $value $value;
    setting the switches 10101010
    root@zedboard:/etc/init.d# read_sw
    0xaa 170

    I recently built a system.bit and with meta-topic a fpga.bin
    It appears that the fpga.bin is being loaded since I have a script
    ck_fpga  that I extracted from /etc/init.d/fpga-image-load.sh
    #!/bin/sh
    #extracted from /etc/init.d/fpga-image-load.sh
    #used to check if fpga.bin was loaded.
    result=`cat     /sys/devices/amba.[0123]/f8007000.devcfg/prog_done`
    echo $result
    root@zedboard:~# ./ck_fpga
    1

    I would think that 8 Leds would be 73-80.
    cat /usr/bin/export_led
    #!/bin/bash
    #This appears to work with fpga.bin loaded
    echo "++ Exporting switches "
    for i in 0 1 2 3 4 5 6 7 ;
    do
            led=$(($i+73));
            echo $led > /sys/class/gpio/export;
            echo out > /sys/class/gpio/gpio$led/direction;
    done;
    This gets errors.
    Could this be the problem ZedBoard_Linux_Design net processing_system7_0_GPIO<7>  LOC = T22 while the
    cf_adv7511_zed uses NET processing_system7_0_GPIO_pin[11].  I have gone over this many times but can not determine the offsets needed to get the 8 Leds to work.   Any and all help is appreciated. Thanks
                                               ZedBoard_Linux_Design
    system.ucf
    ############################
    #                          #
    # On-board LED's           #
    #                          #
    ############################
    net processing_system7_0_GPIO<7>  LOC = T22 | IOSTANDARD = LVCMOS33;    # LD0
    net processing_system7_0_GPIO<8>  LOC = T21 | IOSTANDARD = LVCMOS33;    # LD1
    net processing_system7_0_GPIO<9>  LOC = U22 | IOSTANDARD = LVCMOS33;    # LD2
    net processing_system7_0_GPIO<10> LOC = U21 | IOSTANDARD = LVCMOS33;    # LD3
    net processing_system7_0_GPIO<11> LOC = V22 | IOSTANDARD = LVCMOS33;    # LD4
    net processing_system7_0_GPIO<12> LOC = W22 | IOSTANDARD = LVCMOS33;    # LD5
    net processing_system7_0_GPIO<13> LOC = U19 | IOSTANDARD = LVCMOS33;    # LD6
    net processing_system7_0_GPIO<14> LOC = U14 | IOSTANDARD = LVCMOS33;    # LD7

    ############################
    #                          #
    # On-board Slide Switches  #
    #                          #
    ############################
    net processing_system7_0_GPIO<15> LOC = F22 | IOSTANDARD = LVCMOS33;    # SW0
    net processing_system7_0_GPIO<16> LOC = G22 | IOSTANDARD = LVCMOS33;    # SW1
    net processing_system7_0_GPIO<17> LOC = H22 | IOSTANDARD = LVCMOS33;    # SW2
    net processing_system7_0_GPIO<18> LOC = F21 | IOSTANDARD = LVCMOS33;    # SW3
    net processing_system7_0_GPIO<19> LOC = H19 | IOSTANDARD = LVCMOS33;    # SW4
    net processing_system7_0_GPIO<20> LOC = H18 | IOSTANDARD = LVCMOS33;    # SW5
    net processing_system7_0_GPIO<21> LOC = H17 | IOSTANDARD = LVCMOS33;    # SW6
    net processing_system7_0_GPIO<22> LOC = M15 | IOSTANDARD = LVCMOS33;    # SW7
    GPIO
        MIO GPIO MIO
            EMIO GPIO (Width) 60
    MIO 0   GPIO gpio[0] disabled
    MIO 9   GPIO gpio[9] disabled
    MIO 10   GPIO gpio[10] disabled
               .
               .
               .
    MIO 15   GPIO gpio[15] disabled
    Ports
                  Connected Port
    (IO_IF)GPIO_0 Connected to External Ports
                  External Posts::processing_system7_0_MIO
           GPIO   External Posts::processing_system7_0_GPIO IO [59:0]
           GPIO_I                                             I [59:0]
           GPIO_O                                             O [59:0]
           GPIO_T                                             O [59:0]


                                               cf_adv7511_zed
    system.ucf
    NET processing_system7_0_GPIO_pin[11]    LOC = F22  | IOSTANDARD="LVCMOS25";  # "SW0"
    NET processing_system7_0_GPIO_pin[12]    LOC = G22  | IOSTANDARD="LVCMOS25";  # "SW1"
    NET processing_system7_0_GPIO_pin[13]    LOC = H22  | IOSTANDARD="LVCMOS25";  # "SW2"
    NET processing_system7_0_GPIO_pin[14]    LOC = F21  | IOSTANDARD="LVCMOS25";  # "SW3"
    NET processing_system7_0_GPIO_pin[15]    LOC = H19  | IOSTANDARD="LVCMOS25";  # "SW4"
    NET processing_system7_0_GPIO_pin[16]    LOC = H18  | IOSTANDARD="LVCMOS25";  # "SW5"
    NET processing_system7_0_GPIO_pin[17]    LOC = H17  | IOSTANDARD="LVCMOS25";  # "SW6"
    NET processing_system7_0_GPIO_pin[18]    LOC = M15  | IOSTANDARD="LVCMOS25";  # "SW7"

    NET processing_system7_0_GPIO_pin[19]    LOC = T22  | IOSTANDARD="LVCMOS33";  # "LD0"
    NET processing_system7_0_GPIO_pin[20]    LOC = T21  | IOSTANDARD="LVCMOS33";  # "LD1"
    NET processing_system7_0_GPIO_pin[21]    LOC = U22  | IOSTANDARD="LVCMOS33";  # "LD2"
    NET processing_system7_0_GPIO_pin[22]    LOC = U21  | IOSTANDARD="LVCMOS33";  # "LD3"
    NET processing_system7_0_GPIO_pin[23]    LOC = V22  | IOSTANDARD="LVCMOS33";  # "LD4"
    NET processing_system7_0_GPIO_pin[24]    LOC = W22  | IOSTANDARD="LVCMOS33";  # "LD5"
    NET processing_system7_0_GPIO_pin[25]    LOC = U19  | IOSTANDARD="LVCMOS33";  # "LD6"
    NET processing_system7_0_GPIO_pin[26]    LOC = U14  | IOSTANDARD="LVCMOS33";  # "LD7"
    GPIO
        MIO GPIO MIO
            EMIO GPIO (Width) 32
    MIO 0   GPIO gpio[0] disabled
    MIO 9   GPIO gpio[9] disabled
    MIO 10   GPIO gpio[10] disabled
               .
               .
               .
    MIO 15   GPIO gpio[15] disabled
    Ports
                  Connected Port
    (IO_IF)GPIO_0 Connected to External Ports
           GPIO   External Posts::processing_system7_0_GPIO_pin IO [31:0]
           GPIO_I                                             I [31:0]
           GPIO_O                                             O [31:0]
           GPIO_T                                             O [31:0]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data