Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Difficulty booting Ubuntu on Aedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 842 views
  • Users 0 members are here
  • zedboard
Related

Difficulty booting Ubuntu on Aedboard

vivekgov
vivekgov over 6 years ago

Hi, I currently have difficulty in getting Ubuntu running on my zedboard. I am using the tutorial 'Zedboard Ubuntu, Vivado 2013.4' which I obtained from | Zedboard . I'm using Vivado 2013.4 as well as CentOS8 as my Virtual machine with Windows 10 as my host. My problem is that at the final stage(experiment 8) my zedboard fails to boot with ubuntu. The error that is displayed from teraterm is as follows-

 

Device: zynq_sdhci

Manufacturer ID: 3

OEM: 5344

Name: SU04G

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 3.7 GiB

Bus Width: 4-bit

reading uEnv.txt

** Unable to read file uEnv.txt **

Copying Linux from SD to RAM...RFS in ext4...

reading uImage

2946168 bytes read in 282 ms (10 MiB/s)

reading devicetree.dtb

9802 bytes read in 14 ms (683.6 KiB/s)

## Booting kernel from Legacy Image at 03000000 ...

   Image Name:   Linux-3.13.0-g5aa6400

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2946104 Bytes = 2.8 MiB

   Load Address: 00008000

   Entry Point:  00008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 02a00000

   Booting using the fdt blob at 0x2a00000

   Loading Kernel Image ... OK

   Loading Device Tree to 1fb29000, end 1fb2e649 ... OK

 

 

Starting kernel ...

 

 

Uncompressing Linux... done, booting the kernel.

Booting Linux on physical CPU 0x0

Linux version 3.13.0-g5aa6400 (ron@ubuntu) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #1 SMP PREEMPT Thu Apr 24 15:16:47 PDT 2014

CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Xilinx Zynq ZED

bootconsole [earlycon0] enabled

cma: CMA: reserved 40 MiB at 1d000000

Memory policy: Data cache writealloc

PERCPU: Embedded 7 pages/cpu @c09e2000 s7616 r8192 d12864 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048

Kernel command line: = console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 472628K/524288K available (3922K kernel code, 237K rwdata, 1484K rodata, 183K init, 128K bss, 51660K reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)

    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc054fb08   (5407 kB)

      .init : 0xc0550000 - 0xc057ddc0   ( 184 kB)

      .data : 0xc057e000 - 0xc05b9440   ( 238 kB)

       .bss : 0xc05b944c - 0xc05d94a4   ( 129 kB)

Preemptible hierarchical RCU implementation.

        Dump stacks of tasks blocking RCU-preempt GP.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

NR_IRQS:16 nr_irqs:16 16

slcr mapped to e0802000

Zynq clock init

sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207951633ns

timer #0 at e0804000, irq=43

Console: colour dummy device 80x30

Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x3b4518 - 0x3b454c

L310 cache controller enabled

l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 512 kB

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

Brought up 2 CPUs

SMP: Total of 2 processors activated.

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

regulator-dummy: no parameters

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

zynq-gpio e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080e000

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

zynq-ocm fffc0000.ps7-ocm: ZYNQ OCM pool: 256 KiB @ 0xe0880000

zynq-ocm fffc0000.ps7-ocm: can't request region for resource [mem 0xfffc0000-0xffffffff]

zynq-ocm: probe of fffc0000.ps7-ocm failed with error -16

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

media: Linux media interface: v0.10

Linux video capture interface: v2.00

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource ttc_clocksource

NET: Registered protocol family 2

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 4096 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

TCP: reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

msgmni has been set to 1003

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

dma-pl330 f8003000.ps7-dma: Loaded driver for PL330 DMAC-2364208

dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16

e0001000.uart: ttyPS0 atconsole [ttyPS0] enabled

console [ttyPS0] enabled

bootconsole [earlycon0] disabled

bootconsole [earlycon0] disabled

xdevcfg f8007000.devcfg: ioremap 0xf8007000 to e0814000

[drm] Initialized drm 1.1.0 20060810

platform 70e00000.axi_hdmi: Driver axi-hdmi requests probe deferral

brd: module loaded

loop: module loaded

zynq-qspi e000d000.qspi: master is unqueued, this is deprecated

m25p80 spi32766.0: found s25fl256s1, expected m25p80

m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)

5 ofpart partitions found on MTD device spi32766.0

Creating 5 MTD partitions on "spi32766.0":

0x000000000000-0x000000500000 : "boot"

0x000000500000-0x000000520000 : "bootenv"

0x000000520000-0x000000540000 : "config"

0x000000540000-0x000000fc0000 : "image"

0x000000fc0000-0x000002000000 : "spare"

zynq-qspi e000d000.qspi: at 0xE000D000 mapped to 0xE0816000, irq=51

libphy: XEMACPS mii bus: probed

xemacps e000b000.eth: pdev->id -1, baseaddr 0xe000b000, irq 54

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ULPI transceiver vendor/product ID 0x0451/0x1507

Found TI TUSB1210 ULPI transceiver.

ULPI integrity check: passed.

zynq-ehci zynq-ehci.0: Xilinx Zynq USB EHCI Host Controller

zynq-ehci zynq-ehci.0: new USB bus registered, assigned bus number 1

zynq-ehci zynq-ehci.0: irq 53, io mem 0x00000000

zynq-ehci zynq-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usbserial

usbcore: registered new interface driver usbserial_generic

usbserial: USB Serial support registered for generic

usbcore: registered new interface driver ftdi_sio

usbserial: USB Serial support registered for FTDI USB Serial Device

mousedev: PS/2 mouse device common for all mice

i2c /dev entries driver

zynq-wdt f8005000.swdt: Xilinx Watchdog Timer at e081c000 with timeout 10s

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

sdhci-arasan e0100000.sdhci: dummy supplies not allowed

mmc0: no vqmmc regulator found

sdhci-arasan e0100000.sdhci: dummy supplies not allowed

mmc0: no vmmc regulator found

mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA

ledtrig-cpu: registered to indicate activity on CPUs

hidraw: raw HID events driver (C) Jiri Kosina

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

adv7511-hdmi-snd adv7511_hdmi_snd.4: adv7511 <-> 75c00000.axi-spdif-tx mapping ok

mmc0: new high speed SDHC card at address e624

mmcblk0: mmc0:e624 SU04G 3.69 GiB

mmcblk0: p1 p2

zed-adau1761-snd zed_sound.5: adau-hifi <-> 77600000.axi-i2s mapping ok

TCP: cubic registered

NET: Registered protocol family 17

Registering SWP/SWPB emulation handler

axi-hdmi 70e00000.axi_hdmi: No connectors reported connected with modes

[drm] Cannot find any crtc or sizes - going 1024x768

Console: switching to colour frame buffer device 128x48

axi-hdmi 70e00000.axi_hdmi: fb0:  frame buffer device

axi-hdmi 70e00000.axi_hdmi: registered panic notifier

[drm] Initialized axi_hdmi_drm 1.0.0 20120930 on minor 0

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

ALSA device list:

  #0: HDMI monitor

  #1: ZED ADAU1761

JBD2: Unrecognised features on journal

EXT4-fs (mmcblk0p2): error loading journal

List of all partitions:

1f00            5120 mtdblock0  (driver?)

1f01             128 mtdblock1  (driver?)

1f02             128 mtdblock2  (driver?)

1f03           10752 mtdblock3  (driver?)

1f04           16640 mtdblock4  (driver?)

b300         3872256 mmcblk0  driver: mmcblk

  b301           53248 mmcblk0p1 34c47715-01

  b302         3814400 mmcblk0p2 34c47715-02

No filesystem could mount root, tried:  ext4

Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)

CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.13.0-g5aa6400 #1

[<c00135d8>] (unwind_backtrace+0x0/0xe0) from [<c0010ab4>] (show_stack+0x10/0x14)

[<c0010ab4>] (show_stack+0x10/0x14) from [<c03afc34>] (dump_stack+0x78/0xc8)

[<c03afc34>] (dump_stack+0x78/0xc8) from [<c03ae2cc>] (panic+0x84/0x1d8)

[<c03ae2cc>] (panic+0x84/0x1d8) from [<c0550fcc>] (mount_block_root+0x244/0x290)

[<c0550fcc>] (mount_block_root+0x244/0x290) from [<c05512bc>] (prepare_namespace+0x15c/0x1bc)

[<c05512bc>] (prepare_namespace+0x15c/0x1bc) from [<c0550c38>] (kernel_init_freeable+0x178/0x1c0)

[<c0550c38>] (kernel_init_freeable+0x178/0x1c0) from [<c03acf98>] (kernel_init+0x8/0x100)

[<c03acf98>] (kernel_init+0x8/0x100) from [<c000db38>] (ret_from_fork+0x14/0x3c)

CPU1: stopping

CPU: 1 PID: 0 Comm: swapper/1 Not tainted 3.13.0-g5aa6400 #1

[<c00135d8>] (unwind_backtrace+0x0/0xe0) from [<c0010ab4>] (show_stack+0x10/0x14)

[<c0010ab4>] (show_stack+0x10/0x14) from [<c03afc34>] (dump_stack+0x78/0xc8)

[<c03afc34>] (dump_stack+0x78/0xc8) from [<c0012010>] (ipi_cpu_stop+0x3c/0x68)

[<c0012010>] (ipi_cpu_stop+0x3c/0x68) from [<c00126ac>] (handle_IPI+0x5c/0x7c)

[<c00126ac>] (handle_IPI+0x5c/0x7c) from [<c00084d4>] (gic_handle_irq+0x50/0x58)

[<c00084d4>] (gic_handle_irq+0x50/0x58) from [<c0011580>] (__irq_svc+0x40/0x70)

Exception stack(0xdcc85fa0 to 0xdcc85fe8)

5fa0: c09ea718 00000000 00000000 00000000 dcc84000 c05b934b c0586464 c03b6c40

5fc0: 0000406a 413fc090 00000000 00000000 00000000 dcc85fe8 c000e62c c000e630

5fe0: 60000113 ffffffff

[<c0011580>] (__irq_svc+0x40/0x70) from [<c000e630>] (arch_cpu_idle+0x24/0x2c)

[<c000e630>] (arch_cpu_idle+0x24/0x2c) from [<c004d9a4>] (cpu_startup_entry+0xa8/0x10c)

[<c004d9a4>] (cpu_startup_entry+0xa8/0x10c) from [<00008564>] (0x8564)

drm_kms_helper: panic occurred, switching back to text console

 

 

I have done everything as stated in the tutorial, but I still receive this error. When I checked appendix 5 its written that the kernel panic occurs when the rootfs is not present in the ext4 second partition. I partitioned the sd card using gparted in centos and have extracted the linaro ubuntu files into the second ext4 partition. Upon searching online I found a solution here- https://stackoverflow.com/questions/50220156/error-in-booting-from-usd-card-no-filesystem-could-mount-root-triedext4

Using the solution there I canceled the autoboot and entered the command suggested,setenv bootargs console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait, and saveenv. It boots and then freezes at booting kernel

 

 

 

Device: zynq_sdhci

Manufacturer ID: 3

OEM: 5344

Name: SU04G

Tran Speed: 50000000

Rd Block Len: 512

SD version 3.0

High Capacity: Yes

Capacity: 3.7 GiB

Bus Width: 4-bit

reading uEnv.txt

** Unable to read file uEnv.txt **

Copying Linux from SD to RAM...RFS in ext4...

reading uImage

2946168 bytes read in 282 ms (10 MiB/s)

reading devicetree.dtb

9802 bytes read in 14 ms (683.6 KiB/s)

## Booting kernel from Legacy Image at 03000000 ...

   Image Name:   Linux-3.13.0-g5aa6400

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2946104 Bytes = 2.8 MiB

   Load Address: 00008000

   Entry Point:  00008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 02a00000

   Booting using the fdt blob at 0x2a00000

   Loading Kernel Image ... OK

   Loading Device Tree to 1fb29000, end 1fb2e649 ... OK

 

 

Starting kernel ...

 

 

Uncompressing Linux... done, booting the kernel.

 

It would be great if someone could help me with this. I'd also like to mention that I used the prebuilt files provided in the tutorial for the first fat32 partition, which are the three files boot.bin, devicetree.dtb and uImage. I did so because I had difficulties using the arm cross compiler in Linux. Thanks in advance!

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    You might need to ask this question over at Digilent's forums.  We do not really support Ubuntu nor tools under CentOS8.  Even the most CURRENT Xilinx tools only work up to CentOS7.

    https://xilinx.github.io/Vitis_Libraries/quantitative_finance/overview.html

     

    --Dan