Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zynq reads the internal temperature of the PHY chip.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 359 subscribers
  • Views 1991 views
  • Users 0 members are here
  • zedboard
Related

Zynq reads the internal temperature of the PHY chip.

jun_ling_
jun_ling_ over 5 years ago

Hi folks:

 

I am planning to write code on the PS (ARM) side to read the temperature of the PHY chip, namely, Marvell 88E1512 (eth0) on the zedboard, but to no avail.

Datasheet of the Marvell 88E1512 chip states that one "can read the temperature from register_26_6.4:0 or register_27_6.7:0". The data read  from there (by calling ioctl(socket, SIOCSMIIREG, &reg_info) ), unfortunately, is either 0x0000 or 0xFFFF.

What is the best practice to achieve this? Any input / recommendation would be greatly appreciated.

 

Additionally, what is the difference between phy_id and page?

 

Thank you for reading.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago in reply to jun_ling_ +1 verified
    I've had a very quick look at your code - I don't have time to pick through it all but: The phy has an ID, that's in case there are more than one on the MDIO bus, Inside the phy are several pages of registers…
Parents
  • michaelkellett
    0 michaelkellett over 5 years ago

    Have you set the page address ?

    Register 22 in any page sets the page to be accessed.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jun_ling_
    0 jun_ling_ over 5 years ago in reply to michaelkellett

    #include <stdio.h>
    #include <stdlib.h>
    #include <string.h>
    #include <linux/mii.h>
    #include <sys/types.h>
    #include <sys/socket.h>
    #include <sys/ioctl.h>
    #include <net/if.h>
    #include <linux/sockios.h>
    #include <linux/types.h>
    #include <netinet/in.h>
    #include <unistd.h>
    #include <time.h>
    
    struct mii_ioctl_data
    {
        __u16 phy_id;
        __u16 reg_num;
        __u16 val_in;
        __u16 val_out;
    }
    
    void help()
    {
        printf("mdio:\n");
        printf("read operation: mdio phy_addr reg_addr\n");
        printf("write operation: mdio  phy_addr reg_addr value\n");
        printf("For example:\n");
        printf("mdio eth0 6 27\n");
        printf("mdio eth0 6 27 0x12\n\n");
    }
    
    
    int main(int nArgc, char *pArgv[])
    {
        if (nArgc == 1 || !strcmp(pArgv[1], "-h"))
        {
            help();
            return 0;
        }
    
        struct mii_ioctl_data *pMiiData = NULL;
        struct ifreq oRegInfo;
        memset(&oRegInfo, 0, sizeof(oRegInfo));
        strncpy(oRegInfo.ifr_name, pArgv[1], IFNAMSIZ - 1);
        printf("ifreq name : %s\n", oRegInfo.ifr_name);
    
        int nRet = 0;
        int nSockFd = -1;
    
        do
        {
            nSockFd = socket(PF_LOCAL, SOCK_DGRAM, 0);
            if (nSockFd < 0)
            {
                break;
            }
            // get phy address in smi bus
            printf("Get phy address in smi bus...\n");
            nRet = ioctl(nSockFd, SIOCGMIIPHY, &oRegInfo);
            if (nRet < 0)
            {
                break;
            }
    
            pMiiData = (struct mii_ioctl_data*) &oRegInfo.ifr_data;
            if (4 == nArgc)
            {
                pMiiData->phy_id = (uint16_t) strtoul(pArgv[2], NULL, 0);;
                pMiiData->reg_num = (uint16_t) strtoul(pArgv[3], NULL, 0);
                printf("pht_id = %d, reg_num = %d\n", pMiiData->phy_id , pMiiData->reg_num);
    
                for (int nIdx = 0; nIdx != 1000; ++nIdx)
                {
                    nRet = ioctl(nSockFd, SIOCGMIIREG, &oRegInfo);
                    if (nRet < 0)
                    {
                        printf("get register value failed\n");
                        break;
                    }
                    printf("read phy addr: 0x%x reg: 0x%x value : 0x%x\n\n",
                    pMiiData->phy_id, pMiiData->reg_num, pMiiData->val_out);
                    int nTempValue = ((pMiiData->val_out & 0xFF) - 25) * 1000;
                    printf("Round %d temperature : %d\n", nIdx, nTempValue);
    
                    struct timespec t;
                    t.tv_sec = 1;
                    t.tv_nsec = 0;
                    nanosleep(&t, NULL);
                }
            }
            else if (5 == nArgc)
            {
                pMiiData->phy_id = (uint16_t) strtoul(pArgv[2], NULL, 0);;
                pMiiData->reg_num = (uint16_t) strtoul(pArgv[3], NULL, 0);
                pMiiData->val_in = (uint16_t) strtoul(pArgv[4], NULL, 0);
                printf("pht_id = %d, reg_num = %d, set_value = %d\n", pMiiData->phy_id , pMiiData->reg_num, pMiiData->val_in);
                nRet = ioctl(nSockFd, SIOCSMIIREG, &oRegInfo);
                if (nRet < 0)
                {
                    printf("set register value failed\n");
                    break;
                }
                printf("write phy addr: 0x%x reg: 0x%x value : 0x%x\n\n",
                pMiiData->phy_id, pMiiData->reg_num, pMiiData->val_in);
    
                for (int nIdx = 0; nIdx != 1000; ++nIdx)
                {
                    nRet = ioctl(nSockFd, SIOCGMIIREG, &oRegInfo);
                    if (nRet < 0)
                    {
                        printf("get register value failed\n");
                        break;
                    }
                    printf("read phy addr: 0x%x reg: 0x%x value : 0x%x\n\n",
                    pMiiData->phy_id, pMiiData->reg_num, pMiiData->val_out);
    
                    int nTempValue = ((pMiiData->val_out & 0xFF) - 25) * 1000;
                    printf("Round %d temperature : %d\n", nIdx, nTempValue);
    
                    struct timespec t;
                    t.tv_sec = 1;
                    t.tv_nsec = 0;
                    nanosleep(&t, NULL);
                }
            }
        } while (0);
    
        if (nSockFd >= 0)
        {
            close(nSockFd);
            nSockFd = -1;
        }
        return 0;
    }

     

    My code goes like this. Input argument examples are provided in sub-function HELP starting on line 23 above.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to jun_ling_

    I've had a very quick look at your code  - I don't have time to pick through it all but:

     

    The phy has an ID, that's in case there are more than one on the MDIO bus,

    Inside the phy are several pages of registers, and the page you get access to depends on what is in register 22 which is common to all pages

     

    Your code only seems to set phy_id and reg_num to access registers - you have to look after the page as well.

     

    Find some registers on different pages in the data sheet and check the contents. Then adjust register 22 and do it again.

    I think you'll find that you are operating with register 22 set to zero (power up default).

     

    The Marvel data sheet does describe all this (I can't quite go so far as to suggest that it explains any of it very well image)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 5 years ago in reply to jun_ling_

    I've had a very quick look at your code  - I don't have time to pick through it all but:

     

    The phy has an ID, that's in case there are more than one on the MDIO bus,

    Inside the phy are several pages of registers, and the page you get access to depends on what is in register 22 which is common to all pages

     

    Your code only seems to set phy_id and reg_num to access registers - you have to look after the page as well.

     

    Find some registers on different pages in the data sheet and check the contents. Then adjust register 22 and do it again.

    I think you'll find that you are operating with register 22 set to zero (power up default).

     

    The Marvel data sheet does describe all this (I can't quite go so far as to suggest that it explains any of it very well image)

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jun_ling_
    0 jun_ling_ over 5 years ago in reply to michaelkellett

    Hi MK:

     

    Thanks for the tip, and that does the trick.