Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard rev. F DDR3
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 1518 views
  • Users 0 members are here
  • zedboard_hardware
  • ps ddr
  • zedboard rev. f
Related

Zedboard rev. F DDR3

xabn
xabn over 4 years ago

Hi,

 

I would like to assure the DDR3 used in Zedboard rev. F.

As fas as I know, rev. C comes with MT41J128M16HA-15E:D 1, while rev. D 2 comes with MT41K128M16JT-125:K.

 

In vivado project, I cannot find the exact part number of the last one (I do not know what K means). Moreover the last one seems to be a low voltage DDR3 (SDRAM - DDR3L) and its max. voltage is 1.45 V (instead of 1.5V of the schematics).

 

Any help on this? Should I use in Vivado MT41K128M16JT-125 part for Zedboard rev. F??

 

image

 

Many thanks in advance,

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 4 years ago

    Typically, a new DDR part is specifically selected to be fully backwards compatible with the previous boards. I would be very surprised if Digilent did something different this time. Therefore, I suggest you use the DDR settings that are captured in the board definition file.

     

    Additionally, the settings you populate in Vivado must be the maximum settings allowed by both the DDR and the Xilinx device. Many times, the Xilinx controller is the limitation, not the DDR, at least when it comes to frequency. Again, use the published board definition and you should be OK.

     

    Bryan