Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZEDBOARD UART-USB connection problem in linux while using matlab
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 358 subscribers
  • Views 1741 views
  • Users 0 members are here
  • zedboard
  • serialport
  • matlab
  • uart
  • hdlcoder
Related

ZEDBOARD UART-USB connection problem in linux while using matlab

Rohith_Gopakumar
Rohith_Gopakumar over 2 years ago

hello i am new to zedboard and am trying to set up the hardware since the past few weeks so any help would be great. i am trying to connect the board to the development computer

TOOL VERSIONS:

matlab version-R2022b

os-Ubuntu 20.04.3 LTS

i have used HDL Coder Support Package for Xilinx Zynq Platform

 

I keep getting this error and i'm not sure how to resolve it, any and all help would be appreciated thank you

----------------------------------------------------------------------------------------------------------------------------------------------

attempts done:

1)i have tried to setup serial port using s=serialport('dev/ttyACM0',115200);  fopen(s) then tried the hardware

2)i have given permissions for dev/ttyACM0 by chmod 666

3)i have used putty to communicate with the zynq board

image

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 2 years ago

    Hi,

    I know nothing about zedboard so I probably cannot help, however, so that others can help you, you may need to supply a bit more information.

    You have not shown an error. All I see are warnings. The output on the display actually looks fine so far. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • flyingbean
    0 flyingbean over 2 years ago

    Not many peoples here using Matlab to run FPGA and communicate UART via Matlab/FPGA.  In the meanwhile you used Linux for Matlab toolchain, which making the pool of the similar designers as you even less. You might need to ask help at Mathwork. Here is a snapshot from Mathwork about a similar question as yours.

    image

    Looks like the buffer size of UART could be a stopper after the communication starting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Rohith_Gopakumar
    0 Rohith_Gopakumar over 2 years ago in reply to shabaz

    I am following a matlab simulink tutorial and in that serialport was also displayed. This was the output in the video but he was using windows so i was really confused why it up wasn't shown in my setup.

    imageThis is the output from the tutorial.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Rohith_Gopakumar
    0 Rohith_Gopakumar over 2 years ago in reply to flyingbean

    I am able to connect using putty to the zedboard, so the communication is possible. One of the explainations i found was that matlab only recognises ttyS*, which is a very small portion of the ones present in linux and from what i figured out mine used DEV/ttyACM0. 

    i tried creating a link to ttyS101 and then trying to set-up but it didn't work.

    I have contacted the mathworks support but any help from here would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dyessgg
    0 dyessgg over 2 years ago in reply to Rohith_Gopakumar

    I'm not an expert so I don't know the exact way to do this, but maybe try creating a udev rule to name the serial port as you wish.

    There might be a Device Tree entry that will tell the serial driver on the ZEDBoard to generate a /dev/ttyS name. 

    If all else fails, modify the particular serial driver to create a name you want.

    Unless I am completely misunderstanding the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Rohith_Gopakumar
    0 Rohith_Gopakumar over 2 years ago in reply to dyessgg

    I had use sudo ln -s /dev/ttyACM0 /dev/ttyS101 to create a symbolic link 

    i used this as reference so please do correct me if my understanding was wrong in any way.