Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard troubleshooting : Power LED and DONE LED does not turn ON
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 1262 views
  • Users 0 members are here
Related

Zedboard troubleshooting : Power LED and DONE LED does not turn ON

teem-8121
teem-8121 over 1 year ago

The zedboard was working all fine.

But suddenly the Power LED, DONE LED, does not turn ON when 12V adaptor is plugged in with Switch ON, whereas the LD0 to LD7 stays ON in red when the board is powered.

I checked for the voltage across the following Capacitors with a DMM while the Zedboard is powered:
C328, C329 or C330 ( should be 5V)
C334 or C335 ( should be 3.3V)
C351 or C352 ( should be 1.5V)
C365 or C366 ( should be 1.8V)
C356 or C357 ( should be 1V)
I also verified the fuse voltage F5 and the switch SW8
All of these measured as expected. Not sure what could have went wrong.


Could you suggest some more steps to troubleshoot?

  • Sign in to reply
  • Cancel
Parents
  • bidrohini
    0 bidrohini over 1 year ago

    Recheck the PGOOD (Power Good) signals associated with different voltage rails. If the PGOOD signals aren’t asserted correctly, the board may not proceed with its boot sequence. This is why the DONE LED is not illuminating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bidrohini
    0 bidrohini over 1 year ago

    Recheck the PGOOD (Power Good) signals associated with different voltage rails. If the PGOOD signals aren’t asserted correctly, the board may not proceed with its boot sequence. This is why the DONE LED is not illuminating.