Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Je1 GPIO - Cant seem to access upper pins
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 595 views
  • Users 0 members are here
Related

Je1 GPIO - Cant seem to access upper pins

PurplePig
PurplePig over 1 year ago
# Xilinx Zedboard (Zynq 7020) GPIO 0

I am working with a new Zedboard with the Zynq 7020 processor.

I was trying to strobe the pins on the JE1 PMOD port

image

 To this end I defined the following pins



```
File: helloworld.c

61: int             iPortPins[10];
62:
63: #define JE1     13
64: #define JE2     10
65: #define JE3     11
66: #define JE4     12
67: #define JE7     0
68: #define JE8     9
69: #define JE9     14
70: #define JE10    15
71: #define LED     7
72:

```

and configured them as follows

image

defined as

image

what I had observed as that the GPIO_0 DIRM and OEN were not allowing the GPIO 0 pins to
drive the PMOD so I explicitly set them

What I observed is I was only able to write the lower 8 bits of each of these registers.

image



### before
image

code to change **DIRM** and **OEN**

```
        u32 pGPIO_0_DIRM = 0xE000A204;
        Xil_Out32(pGPIO_0_DIRM, (u32)(iMask));

        u32 pGPIO_0_OEN = 0xE000A208;
        Xil_Out32(pGPIO_0_OEN, (u32)(iMask));
```

### after
image

Note that bits 8-15 were ignored.

This is also the case if I try to modify them from the ide memory window. If I write 0xffffffff only the lower 8 bits are modified.
(Both DIRM and OEN)

Why is this?



  • Sign in to reply
  • Cancel
  • PurplePig
    PurplePig over 1 year ago

    Source

    /******************************************************************************
    *
    * Copyright (C) 2009 - 2014 Xilinx, Inc.  All rights reserved.
    *
    * Permission is hereby granted, free of charge, to any person obtaining a copy
    * of this software and associated documentation files (the "Software"), to deal
    * in the Software without restriction, including without limitation the rights
    * to use, copy, modify, merge, publish, distribute, sublicense, and/or sell
    * copies of the Software, and to permit persons to whom the Software is
    * furnished to do so, subject to the following conditions:
    *
    * The above copyright notice and this permission notice shall be included in
    * all copies or substantial portions of the Software.
    *
    * Use of the Software is limited solely to applications:
    * (a) running on a Xilinx device, or
    * (b) that interact with a Xilinx device through a bus or interconnect.
    *
    * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
    * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY,
    * FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL
    * XILINX  BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY,
    * WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF
    * OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE
    * SOFTWARE.
    *
    * Except as contained in this notice, the name of the Xilinx shall not be used
    * in advertising or otherwise to promote the sale, use or other dealings in
    * this Software without prior written authorization from Xilinx.
    *
    ******************************************************************************/
    
    /*
     * helloworld.c: simple test application
     *
     * This application configures UART 16550 to baud rate 9600.
     * PS7 UART (Zynq) is not initialized by this application, since
     * bootrom/bsp configures it to baud rate 115200
     *
     * ------------------------------------------------
     * | UART TYPE   BAUD RATE                        |
     * ------------------------------------------------
     *   uartns550   9600
     *   uartlite    Configurable only in HW design
     *   ps7_uart    115200 (configured by bootrom/bsp)
     */
    
    #include <stdio.h>
    #include "platform.h"
    #include "xil_printf.h"
    
    #include "xgpiops.h"
    #include "xparameters.h"
    
    XGpioPs_Config	*psGPIO_Config = NULL;
    XGpioPs 		my_Gpio;
    
    int				Status;
    int				Status2;
    
    int				iPortPins[10];
    
    #define JE1		13
    #define JE2		10
    #define JE3		11
    #define JE4		12
    #define JE7		0
    #define JE8		9
    #define JE9		14
    #define JE10	15
    #define LED		7
    
    void pause(u32 u32Pause)
    {
    	volatile u32 ii = 0;
    	for( ii = 0; ii< u32Pause; )
    	{
    		ii++;
    	}
    }
    
    int main()
    {
    	volatile u32 	ii 		= 0;
    	volatile u32 	iMask 	= 0;
    	int				iPinCount = 0;
    
    	init_platform();
    
    	iPortPins[iPinCount++] = JE1;
    	iPortPins[iPinCount++] = JE2;
    	iPortPins[iPinCount++] = JE3;
    	iPortPins[iPinCount++] = JE4;
    	iPortPins[iPinCount++] = JE7;
    	iPortPins[iPinCount++] = JE8;
    	iPortPins[iPinCount++] = JE9;
    	iPortPins[iPinCount++] = JE10;
    	iPortPins[iPinCount++] = LED;
    
    
        print("Hello World. \n\rBienvenidos!\n\r");
    
    //	SlcrUnlock();
    
    //	u32 pUnlock = 0xF8000008;
    //    Xil_Out32(pUnlock, (u32)(0xdf0d));
    
    //    u32 pMIO_PIN_00 = 0xF8000700;
    //    Xil_Out32(pMIO_PIN_00, (u32)(0x1601));
    //    Xil_Out32(pMIO_PIN_00, (u32)(0x1601));
    //    Xil_Out32(pMIO_PIN_00, (u32)(0x0601));
    
    	psGPIO_Config 		= XGpioPs_LookupConfig( XPAR_PS7_GPIO_0_DEVICE_ID );
        Status 	= XGpioPs_CfgInitialize(&my_Gpio, psGPIO_Config, psGPIO_Config->BaseAddr);
    
        if ((Status == 0) && (Status2 == 0))
        {
    
        	for (ii=0; ii < iPinCount; ii++)
        	{
        		XGpioPs_SetDirectionPin( &my_Gpio, iPortPins[ii], 1);
        		XGpioPs_WritePin( &my_Gpio, iPortPins[ii], 1);
        		iMask = iMask | (1 << iPortPins[ii]);
        	}
    
        	u32 pGPIO_0_DIRM = 0xE000A204;
        	Xil_Out32(pGPIO_0_DIRM, (u32)(iMask));
    
        	u32 pGPIO_0_OEN = 0xE000A208;
        	Xil_Out32(pGPIO_0_OEN, (u32)(iMask));
    
        	while(1)
        	{
    	    	for (ii=0; ii < iPinCount; ii++)
    	    	{
    	    		XGpioPs_SetDirectionPin( &my_Gpio, iPortPins[ii], 1);
    	    		XGpioPs_WritePin( &my_Gpio, iPortPins[ii], 0);
    	    	}
            	pause(10000000);
    
    	    	for (ii=0; ii < iPinCount; ii++)
    	    	{
    	    		XGpioPs_SetDirectionPin( &my_Gpio, iPortPins[ii], 1);
    	    		XGpioPs_WritePin( &my_Gpio, iPortPins[ii], 1);
    	    	}
            	pause(10000000);
        	}
        }
    
        print("Successfully ran Hello World application");
        cleanup_platform();
        return 0;
    }
    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • PurplePig
    PurplePig over 1 year ago

    The memory Viewer was not accurate. I added a printf and hot the expected value. XSCT could not read that address.