Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Je1 GPIO - Cant seem to access upper pins
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 358 subscribers
  • Views 595 views
  • Users 0 members are here
Related

Je1 GPIO - Cant seem to access upper pins

PurplePig
PurplePig over 1 year ago
# Xilinx Zedboard (Zynq 7020) GPIO 0

I am working with a new Zedboard with the Zynq 7020 processor.

I was trying to strobe the pins on the JE1 PMOD port

image

 To this end I defined the following pins



```
File: helloworld.c

61: int             iPortPins[10];
62:
63: #define JE1     13
64: #define JE2     10
65: #define JE3     11
66: #define JE4     12
67: #define JE7     0
68: #define JE8     9
69: #define JE9     14
70: #define JE10    15
71: #define LED     7
72:

```

and configured them as follows

image

defined as

image

what I had observed as that the GPIO_0 DIRM and OEN were not allowing the GPIO 0 pins to
drive the PMOD so I explicitly set them

What I observed is I was only able to write the lower 8 bits of each of these registers.

image



### before
image

code to change **DIRM** and **OEN**

```
        u32 pGPIO_0_DIRM = 0xE000A204;
        Xil_Out32(pGPIO_0_DIRM, (u32)(iMask));

        u32 pGPIO_0_OEN = 0xE000A208;
        Xil_Out32(pGPIO_0_OEN, (u32)(iMask));
```

### after
image

Note that bits 8-15 were ignored.

This is also the case if I try to modify them from the ide memory window. If I write 0xffffffff only the lower 8 bits are modified.
(Both DIRM and OEN)

Why is this?



  • Sign in to reply
  • Cancel
Parents
  • PurplePig
    PurplePig over 1 year ago

    The memory Viewer was not accurate. I added a printf and hot the expected value. XSCT could not read that address.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • PurplePig
    PurplePig over 1 year ago

    The memory Viewer was not accurate. I added a printf and hot the expected value. XSCT could not read that address.