Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Board Temperature
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 364 subscribers
  • Views 1576 views
  • Users 0 members are here
Related

Board Temperature

adriang
adriang over 3 years ago

Is the ZUBoard supposed to run so hot? The left half (looking into face with Zynq and ethernet pointing down) of the board is really hot to touch (I'm using the recommended 45W adapter). Never handled a board where even the PCB gets this hot. U13, U18, U25 and U26 are the heat sources. Is this normal?  SysMon for both FPGA and ARM report around 50C. Thanks! 

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +1
    FPGA looked fine. Please check the overall current reading if you can use a bench power supplier. The current is very high, which might give you some hint about hardware issue on ZUBoard.
  • Hitulseo
    Hitulseo over 3 years ago +1
    To monitor the temperature of a board, you can use various methods depending on the board and its components. Here are a few common approaches: On-Board Sensors: Many modern boards have built-in…
  • jafoste4
    jafoste4 over 3 years ago +1 suggested
    Hi Adriang, This is normal/expected, the IC's you are refering to are the TDK uPOL switchers which are converting 15V to the various supply voltages for the IO and SOC causing thermal loss/heat generation…
  • flyingbean
    0 flyingbean over 3 years ago

    FPGA looked fine. Please check the overall current reading if you can use a bench power supplier. The current is very high, which might give you some hint about hardware issue on ZUBoard.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Hitulseo
    0 Hitulseo over 3 years ago

    To monitor the temperature of a board, you can use various methods depending on the board and its components. Here are a few common approaches:

    1. On-Board Sensors: Many modern boards have built-in temperature sensors that can provide accurate readings. These sensors are often connected to the board's microcontroller or system management controller. Check the board's documentation or specifications to identify if such sensors are available and how to access their readings.

    2. External Temperature Sensors: If the board doesn't have on-board temperature sensors or if you require additional monitoring points, you can connect external temperature sensors. These sensors can be connected via various interfaces such as I2C or SPI, and their data can be read by the microcontroller or a dedicated temperature monitoring circuit.

    3. Thermal Imaging: In some cases, you may want to visually inspect the temperature distribution across the board. Thermal imaging cameras or infrared thermometers can help you identify hotspots and temperature variations. These tools provide a real-time view of the board's thermal profile.

    Remember to consider safety precautions and ensure that the board and its components are within their specified temperature ranges. Excessive heat can lead to performance degradation, instability, or even permanent damage to the board and its components.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 3 years ago

    Hi Adriang,

    This is normal/expected, the IC's you are refering to are the TDK uPOL switchers which are converting 15V to the various supply voltages for the IO and SOC causing thermal loss/heat generation. The thermal solution on the ZUBoard is minimal to reduce cost of the platform and only covers the SoC. Its intended use is bench top development platform only, and is not recommended for any high heat environments.

    The only way to get away from this heat would be to engineer a custom/expensive heatsink that directly touches these ICs to dissipate heat. Check out the Ultra96V2 passive heatsink for an example of this. That or go with an active solution, but that gets very noisy!

    This board was thoroughly tested in a desktop environment (23C) with a very intensive SoC image and shouldn't have any issues. It will get hot to the touch but will remain within the Junction temperature requirements of the SOC and power supplies for 99% of use cases. If you still have concern, i'd recommend a small fan to push air flow across the top of it, this would greatly reduce the heat.

    -Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • adriang
    0 adriang over 3 years ago in reply to jafoste4

    Thanks Josh for this reply. I assume it will be ok to leave the board running for hours at a time without worrying about overheating with a small fan near those regulators.

    -Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 3 years ago in reply to adriang

    You dont need the fan, but if it provides you with peace of mind go for it! 

    -Josh