Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard Board Temperature
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 364 subscribers
  • Views 1581 views
  • Users 0 members are here
Related

Board Temperature

adriang
adriang over 3 years ago

Is the ZUBoard supposed to run so hot? The left half (looking into face with Zynq and ethernet pointing down) of the board is really hot to touch (I'm using the recommended 45W adapter). Never handled a board where even the PCB gets this hot. U13, U18, U25 and U26 are the heat sources. Is this normal?  SysMon for both FPGA and ARM report around 50C. Thanks! 

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +1
    FPGA looked fine. Please check the overall current reading if you can use a bench power supplier. The current is very high, which might give you some hint about hardware issue on ZUBoard.
  • Hitulseo
    Hitulseo over 3 years ago +1
    To monitor the temperature of a board, you can use various methods depending on the board and its components. Here are a few common approaches: On-Board Sensors: Many modern boards have built-in…
  • jafoste4
    jafoste4 over 3 years ago +1 suggested
    Hi Adriang, This is normal/expected, the IC's you are refering to are the TDK uPOL switchers which are converting 15V to the various supply voltages for the IO and SOC causing thermal loss/heat generation…
Parents
  • flyingbean
    0 flyingbean over 3 years ago

    FPGA looked fine. Please check the overall current reading if you can use a bench power supplier. The current is very high, which might give you some hint about hardware issue on ZUBoard.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • flyingbean
    0 flyingbean over 3 years ago

    FPGA looked fine. Please check the overall current reading if you can use a bench power supplier. The current is very high, which might give you some hint about hardware issue on ZUBoard.