Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZUBoard EMIO Pin number start from which number on ZedBoard Zync 7020 ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 698 views
  • Users 0 members are here
Related

EMIO Pin number start from which number on ZedBoard Zync 7020 ?

trickntreat
trickntreat over 2 years ago

Hey all 

I was working with EMIO and kept a pin to external . (A20) . I read that it was pin 54 in Zync boards. 

So to access first emio we set the pin 54 to high or low whatsoever you want . 

#include <stdio.h>
#include "platform.h"
#include "xil_printf.h"
#include "xgpiops.h"
#include "xparameters.h"

XGpioPs_Config *gpio_config;
XGpioPs gpio;

void init(){
	int status;
	gpio_config = XGpioPs_LookupConfig(XPAR_PS7_GPIO_0_DEVICE_ID);
	status = XGpioPs_CfgInitialize(&gpio, gpio_config, XPAR_PS7_GPIO_0_BASEADDR);
	if(status == XST_SUCCESS)
		xil_printf("Device Init Successful\n");
	else
		xil_printf("Device Init Failed\n");
}

int main()
{
	u32 sw= 0;
    init_platform();
    init();

    print("Starting GPIO EMIO Test\n\r");

    /////////Setting 51 as input
    XGpioPs_SetDirectionPin(&gpio, 51, 0);


    /////////Setting 51 and 54 as Output
    XGpioPs_SetDirectionPin(&gpio, 47, 1);
    XGpioPs_SetDirectionPin(&gpio, 54, 1);

    XGpioPs_SetOutputEnablePin(&gpio ,47 , 1);
    XGpioPs_SetOutputEnablePin(&gpio ,54 , 1);

    while(1){
    	sw = XGpioPs_ReadPin(&gpio,51);

    	XGpioPs_WritePin(&gpio, 47 , sw);
    	XGpioPs_WritePin(&gpio,54,sw);
    	xil_printf("Value read sw0 : %0d \n ",sw);
    	sleep(1);
    }

    cleanup_platform();
    return 0;
}

Btn is at mio pin 51 . 

Internal user led is at pin 47 . 

and A20 external pin connection has been put at 54 . 

But on scope it does not show the pin going high or low . 

Thanks . 

  • Sign in to reply
  • Cancel
  • viktornikolov
    0 viktornikolov over 2 years ago

    I don't see any obvious problem in the source code you shared (I compared it with this code of mine, which I know for sure works).

    I can only speculate there may be an issue in the HW design. I suggest you share screenshot of your Vivado Diagram.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • trickntreat
    0 trickntreat over 2 years ago in reply to viktornikolov

    image

    I have kept the EMIO width to 1 only . 

    image

    This is an auto generated constraints file when i sythesise the project and put the pin number in GUI . 

    Maybe i should try change the constraint file to match the Hw design external pin number ?